cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103zet + fsmc+ssd1963

batist_2008
Associate II
Posted on February 01, 2013 at 08:38

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
frankmeyer9
Associate II
Posted on February 01, 2013 at 10:31

Hello everyone. I have a task to connect stm32f103zet with ssd1963 (rfc57a1-fiw-d-000) using FSMC.

 

Perhaps you can use the STM3210x eval boards from ST as reference, or the STM-LCD board from Olimex. They use FSMC to connect to the TFT driver, and prvide example source code.

 помогите рабобрать�?�?, что не так.

 

Nje ponimaju.