cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103ZE external SRAM optimal setings

abrous3d
Associate II
Posted on January 01, 2013 at 19:57

Hi to all,

I am testing a new board with STM32F103ZE with 4Mbit x 8 / 55nS external low power SRAM (AS6C4008-55STIN from Alliance Semi.). My CPU clock is 72MHZ. I had some doubts about the  FMSC settings regarding setup times etc since it is not clear how they are calculated. After monitoring the bus with my logic analyzer I ended up with the following (working) parameter set :

// ======= Read bus access ======

  p.FSMC_AddressSetupTime = 1;

  p.FSMC_AddressHoldTime = 0;                   // 0 for SRAM

  p.FSMC_DataSetupTime = 1;                     // 87ns CS  56ns WR         

  p.FSMC_BusTurnAroundDuration = 0;             // 0 for SRAM ?

  p.FSMC_CLKDivision = 0;

  p.FSMC_DataLatency = 0;

  p.FSMC_AccessMode = FSMC_AccessMode_A;

  // ======= Write bus access ======

  p1.FSMC_AddressSetupTime = 1;

  p1.FSMC_AddressHoldTime = 0;                   // 0 for SRAM

  p1.FSMC_DataSetupTime = 3;                     // 85ns CS  57ns WR         

  p1.FSMC_BusTurnAroundDuration = 0;             // 0 for SRAM ?

  p1.FSMC_CLKDivision = 0;

  p1.FSMC_DataLatency = 0;

  p1.FSMC_AccessMode = FSMC_AccessMode_A;

Although, it seems ok - and it works ok so far - I am not sure if the setup is suboptimal or -even worse- very close to the edge.

If any of you guys has bigger experience setting up the FMSC I'd like to hear your opinion. 

Thanks in advance,

Angelo

#sram-fsmc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0