cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103c8t6 spi communication with Arduino

ahmed mohamed
Associate II
Posted on April 15, 2017 at 11:42

Hello 

I devolved a code for stm32 as a master and for arduino as a slave , to send a byte through SPI.

But it did not work. I want to know what is the wrong in my code.

STM32 Master Code :

static void SPI_Config(void);

int main()

{

SPI_Config();

for (int z=0 ; z<50 ; z++){

SPI_I2S_SendData(SPI1,'A');

}

return 0;

}

static void SPI_Config(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

SPI_InitTypeDef SPI_InitStructure;

// Configure SPI1_CLKa and SPI1_MOSI

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7;

GPIO_Init(GPIOA, &GPIO_InitStructure);

// SPI1 no remap (NSS/PA4, SCK/PA5, MISO/PA6, MOSI/PA7)

GPIO_PinRemapConfig(GPIO_Remap_SPI1, DISABLE);

// Spi init

/* SPI configuration *****************************************/

SPI_InitStructure.SPI_Direction =

SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler =

SPI_BaudRatePrescaler_64;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 0;

SPI_Init(SPI1, &SPI_InitStructure);

SPI_Cmd(SPI1, ENABLE);

}

Arduino Slave code:

#include <SPI.h>

char buff [50];

volatile byte indx;

volatile boolean process;

void setup (void) {

Serial.begin (115200);

pinMode(MISO, OUTPUT); // have to send on master in so it set as output

SPCR |= _BV(SPE); // turn on SPI in slave mode

indx = 0; // buffer empty

process = false;

SPI.attachInterrupt(); // turn on interrupt

}

ISR (SPI_STC_vect) // SPI interrupt routine

{

byte c = SPDR; // read byte from SPI Data Register

if (indx < sizeof buff) {

buff [indx++] = c; // save data in the next index in the array buff

if (c == '\r') //check for the end of the word

process = true;

}

}

void loop (void) {

if (process) {

process = false; //reset the process

Serial.println (buff); //print the array on serial monitor

indx= 0; //reset button to zero

}

}
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Posted on April 15, 2017 at 17:38

You would need to make sure the TXE (Transmit Empty) flag is asserted before stuffing additional data.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 15, 2017 at 17:53

How can I do This ?

john doe
Lead
Posted on April 15, 2017 at 20:41

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

you don't show your code that actually attempts the tx/rx. how are you handling slave select?

Posted on April 15, 2017 at 23:53

I made the arduino as a slave 

Posted on April 16, 2017 at 01:13

you dont show your code that actually attempts the transmit and/or receive. you are showing the initialization code, which is very helpful so thank you for that. its a good place to start.

among other questions, how are you handling the slave select? in the code you posted above, it shows you chose to handle it in software. that would mean you selected a pin [on the master] as gpio and manipulated it before and after your attempted read/write command.  its completely understandable to do so since apparently leaving it as hardware select, raises slave select with every byte clocked in/out which can work slowly or not at all sometimes. I don't know. I use that pin as a gpio and manipulate it manually before and after a given spi read.

Posted on April 16, 2017 at 11:14

int main(void)

{

/* SPI1 configuration ---------------------------------------*/

SPI_Config();

while (1)

{

/* Wait till Transmit buffer is empty */

while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET)

{

}

/* Send dummy data */

SPI_I2S_SendData(SPI1, 'b');

}

}
Posted on April 16, 2017 at 11:16

This is the Main code 

actually I want you to tell me what is specifically wrong in my code because actually I am not a professional programmer