cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103 spi communication with ad7730 random wrong number

DKari.1
Associate II

I am communicating with ad7730 (24bit adc) using atm32f103ZCT6. I try to read one of the registers of the adc but each time I receive a random wrong figure. The strange thing is that while debugging using serial wire (STLINK) everything is perfect and I receive correct number from ad7730. But when I run the board out of the power source I receive wrong data. Any help is appreciated in advance

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Use a logic analyzer to see what's happening on the line.

If you feel a post has answered your question, please click "Accept as Solution".
S.Ma
Principal

Start with oscilloscope. Digital analyser can only be used once you have viewed the analog world. Ringing, slew rate, etc...

prain
Senior III

Try to increase CS (NSS) assertion/de-assertion time (check ad7730 data sheet).

Also try with lower SPI clock.