2009-12-21 11:00 PM
stm32f103 DMA receive
2011-05-17 4:34 AM
Hello,
In STM32 library for DMA related interrupts I can only see following interrupt sources. - DMA_IT_TC: Transfer complete interrupt mask - DMA_IT_HT: Half transfer interrupt mask - DMA_IT_TE: Transfer error interrupt mask I have used DMA_IT_TC for UART4 TX to put new data in buffer, how can I use this UART4 Rx? Can I get a interrupt on new data received in buffer by DMA? Does any one have a sample program for this? Regards, Prasad2011-05-17 4:34 AM
If you know how many bytes you will receive, configure the DMA, and when it receives the specified number of bits, DMA_IT_TC will raise the same way it does for TX.
(...) DMA_InitStructure7.DMA_MemoryBaseAddr = (uint32_t)pBuffer; DMA_InitStructure7.DMA_BufferSize = (uint32_t)NumByteToRead; (...) I2C_DMACmd(I2C1, ENABLE); /* Enable the DMA Channel7 Transfer Complete IT */ DMA_ITConfig(DMA1_Channel7, DMA_IT_TC, ENABLE); (...)2011-10-10 11:45 AM
I have successufully set up a DMA FIFO in circular mode, to drain the USART when it's RXNE flag is set. I want to change it so that I can do variable len dma's to different buffers. I have implemented this but only the initial DMA cycle fires off.
I there any reason why I can reprogram the DMA controller and enable the engine within the ISAR? Any examples would be helpful Thanks Steve