cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103 14mhz adc clock and prescalers only allow 12mhz?

andrewg
Associate III

hi i'm reviewing rm0008 ref manual for stm32f103 the adc.

accordingly, adc clock max is 14mhz and it takes 14 adc clock cycles for 1 conversion - hence 1msps per ADC.

however, from the RCC section the available prescalers are 2, 4, 6, 8

and if we take 72mhz / 6 that gives 12 mhz

and if we assume it still takes 14 adc clock cycles per conversion, that gives

1m x 12 / 14 ~ 857ksps per adc?

does it still takes 14 adc clock cycles per conversion if the adc clock runs at 12mhz?

in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?

thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

>>in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?

You clock the F1 at 56 MHz?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

>>in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?

You clock the F1 at 56 MHz?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andrewg
Associate III

i see, unfortunately if the F1 is clocked at 56 mhz, usb may not work, as 72 mhz x 2/3 (prescalers) = 48 mhz which is needed by usb.

it seemed this could be a compromise of sorts

thanks for the cool and quick response. i'd make do with 12mhz on the adc clocks