STM32F102C8 ADC3 Interupt routine missing in STM32F10x_StdPeriph_Driver
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-28 3:50 AM
Posted on February 28, 2014 at 12:50
Hi,
I have noticed that anything related to ADC3 interrupts is missing in the STM32F10x_StdPeriph_Driver. Since the RM contains information about it, I added the needed ADC3 interrupt routine and enum value to the library but no interrupt occurs. I'm suspecting that some issue might exist with ADC3 interrupts and I hope someone can help. I have tried to change the startup_stm32f10x_md_vl.s to contain: ... .word RTCAlarm_IRQHandler .word CEC_IRQHandler .word 0 .word 0 .word 0 .word 0 .word ADC3_IRQHandler .word 0 ... .weak ADC3_IRQHandler .thumb_set ADC3_IRQHandler,Default_Handler ... I put a breakpoint into the default handler but it doesn't get stuck there. The ADC1 I'm using in parallel with the same configuration works fine though. Here is the initialization code: int32_t InitADC( void ) { ADC_InitTypeDef ADC_InitStructure; /* PCLK2 is the APB2 clock */ RCC_ADCCLKConfig(RCC_PCLK2_Div8); /* Enable ADC1 clock so that we can talk to it */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE); // ADC 1 /* Put everything back to power-on defaults */ ADC_DeInit(ADC1); ADC_StructInit(&ADC_InitStructure); ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; /* Disable the scan conversion so we do one at a time */ ADC_InitStructure.ADC_ScanConvMode = DISABLE; /* Don't do continuous conversions - do them on demand */ ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; /* Start conversion by software, not an external trigger */ ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; /* Conversions are 12 bit - put them in the lower 12 bits of the result */ ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; /* Say how many channels would be used by the sequencer */ ADC_InitStructure.ADC_NbrOfChannel = 1; /* Now do the setup */ ADC_Init(ADC1, &ADC_InitStructure); ADC_ITConfig(ADC1, ADC_IT_EOC, ENABLE); ADC_RegularChannelConfig(ADC1,ADC_Channel_2,1,ADC_SampleTime_7Cycles5); // ADC3 ADC_DeInit(ADC3); ADC_StructInit(&ADC_InitStructure); ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; /* Disable the scan conversion so we do one at a time */ ADC_InitStructure.ADC_ScanConvMode = DISABLE; /* Don't do continuous conversions - do them on demand */ ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; /* Start conversion by software, not an external trigger */ ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; /* Conversions are 12 bit - put them in the lower 12 bits of the result */ ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; /* Say how many channels would be used by the sequencer */ ADC_InitStructure.ADC_NbrOfChannel = 1; /* Now do the setup */ ADC_Init(ADC3, &ADC_InitStructure); ADC_ITConfig(ADC3, ADC_IT_EOC, ENABLE); ADC_RegularChannelConfig(ADC3,ADC_Channel_9,1,ADC_SampleTime_7Cycles5); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* Enable ADC3 */ ADC_Cmd(ADC3, ENABLE); /* Enable ADC1 reset calibaration register */ ADC_ResetCalibration(ADC1); /* Check the end of ADC1 reset calibration register */ while( ADC_GetResetCalibrationStatus(ADC1) ){ } /* Start ADC1 calibaration */ ADC_StartCalibration(ADC1); /* Check the end of ADC1 calibration */ while( ADC_GetCalibrationStatus(ADC1) ) { } /* Enable ADC3 reset calibaration register */ ADC_ResetCalibration(ADC3); /* Check the end of ADC3 reset calibration register */ while( ADC_GetResetCalibrationStatus(ADC3) ){ } /* Start ADC3 calibaration */ ADC_StartCalibration(ADC3); /* Check the end of ADC3 calibration */ while( ADC_GetCalibrationStatus(ADC3) ) { } // TODO: consider timeouts for calibration waits ADC_SoftwareStartConvCmd(ADC1,ENABLE); ADC_SoftwareStartConvCmd(ADC3,ENABLE); return 0; } uint16_t ADC1ConvertedValue=0; uint16_t ADC3ConvertedValue=0; void ADC1_IRQHandler(void) { ADC_ClearITPendingBit(ADC1, ADC_IT_EOC); ADC1ConvertedValue = ADC_GetConversionValue(ADC1); } void ADC3_IRQHandler(void) { ADC_ClearITPendingBit(ADC3, ADC_IT_EOC); ADC3ConvertedValue = ADC_GetConversionValue(ADC3); }
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-28 4:30 AM
Posted on February 28, 2014 at 13:30
According to this:
http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1031/LN1566/PF216819
your mentioned MCU has only one ADC.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-28 5:19 AM
Posted on February 28, 2014 at 14:19
Right! I suppose I have to use something like scan mode or single sampling of adc channels then.
Thanks.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-28 7:39 AM
Posted on February 28, 2014 at 16:39
Not sure, but I guess you got something wrong.
The device you mentioned has just one ADC, but this ADC has several channels. The basic difference is - all those channels can only be converted sequentially by one ADC, while separate ADCs can run conversions concurrently. If I remember correctly, the F1 ADC works up to 400ksps, far enough for a lot of applications. For the actual available channels and pin mappings of your MCU, consult the reference manual and datasheet.