2013-09-13 12:03 PM
I can get the value from one channel of ADC but now if I use the scan mode how can I get each value?
thanks :)#include <stm32f10x.h>
#include <stm32f10x_gpio.h>
#include <stm32f10x_rcc.h>
#include <stm32f10x_tim.h>
#include <stm32f10x_adc.h>
#include <misc.h>
int
main(
void
)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* TIM3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
/* GPIOA/C/ADC1/AFIO clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC | RCC_APB2Periph_ADC1 | RCC_APB2Periph_AFIO, ENABLE);
/* GPIO PA1-AF */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* GPIO PC9 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
//configure NVIC
NVIC_InitStructure.NVIC_IRQChannel = ADC1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
//configure timer
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_Period = SystemCoreClock/1000 - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* TIM3 TRGO selection */
TIM_SelectOutputTrigger(TIM3, TIM_TRGOSource_Update);
TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE);
TIM_Cmd(TIM3, ENABLE);
/* ADC */
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T3_TRGO;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 2;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_6, 1, ADC_SampleTime_55Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 2, ADC_SampleTime_55Cycles5);
ADC_ITConfig(ADC1, ADC_IT_EOC, ENABLE);
ADC_ExternalTrigConvCmd(ADC1, ENABLE);
ADC_Cmd(ADC1, ENABLE);
// Enable ADC1 reset calibration register
ADC_ResetCalibration(ADC1);
// Check the end of ADC1 reset calibration register
while
(ADC_GetResetCalibrationStatus(ADC1));
// Start ADC1 calibration
ADC_StartCalibration(ADC1);
// Check the end of ADC1 calibration
while
(ADC_GetCalibrationStatus(ADC1));
GPIO_ResetBits(GPIOC, GPIO_Pin_9);
GPIO_SetBits(GPIOC, GPIO_Pin_9);
while
(1)
{}
}
void
ADC1_IRQHandler(
void
)
{
uint16_t ain = ADC_GetConversionValue (ADC);
uint16_t bin = ADC_GetConversionValue (ADC);
ADC_ClearITPendingBit(ADC1 ,ADC_IT_EOC );
}
#ifdef USE_FULL_ASSERT
void
assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
while
(1)
{}
}
#endif
2013-09-13 12:58 PM
There is a single result per conversion, and it scans to the next. The prescribed manner to handle them is to use DMA, and use the TC or HT interrupt as an EOC for ALL.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.