cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0x devices and HTTPs client

Posted on September 14, 2017 at 13:48

(I don't know if i write the post in right sub-forum place).

I face to one issue to get data from one server using port 443. HTTPS for getting data instead HTTP. (First at all , I am newbie with secure connection protocol).

I am using one typical wifi gateway (i.e:HLK-RM08S). This is connected to one TX/RX STM32F030CC UART and then we send data to server..

Now, for getting valid data from server, we use one script developed under python.

( h2 = httplib2.Http(timeout=30, disable_ssl_certificate_validation=True).

I understand that this means that data is sent without encrypting. is it?. We want do same process with one STM32F030CC instead this python script.

How I can face to this issue?. Does exist one library that I can import and it is valid for STM32F030CC device (in general STM32F0xx family?.

Thanks in advance!

Best regards.

Francisco

#stm32f030cc #stm32f0 #http-post #ssl #tls #https #hlk-rm08s
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0