cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0Dicovery : 4 compilation errors with TASKING IDE

jipidi13
Associate II
Posted on May 24, 2013 at 16:11

Hi

I meet 4 compilation errors (see picture below) when running STM32F0discovery FW demo on TASKING IDE !

can you help

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
jipidi13
Associate II
Posted on May 24, 2013 at 16:15

with the picture in attached file

________________

Attachments :

errors_with_TASKING_IDE.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzqc&d=%2Fa%2F0X0000000bQI%2FaVcko1fvVdJiZN0h2cIKcqPwynawq924qNoHPSpkkOU&asPdf=false
frankmeyer9
Associate II
Posted on May 24, 2013 at 16:43

with the picture in attached file

 

With the shaky forum software, attaching pictures is the second best solution.

I don't know the Tasking toolchain, but the label name ''__START'' suggests you omitted to add the startup code to your project. This code provides all the ''hidden'' features between MCU startup and entry to main. Most toolchains provide it as assembler file (*.s file), and include it automatically when creating a project with their ''wizard''.

Nickname306_O
Senior
Posted on May 29, 2013 at 11:27

Hello,

The symbol ''_START'' is called from the vector table in the linker file '' stm32f0xx.lsl '' . In the last versions of TASKING toolchain , this label is replaced by ''Reset_Handler''. Please change this line in your linker file as follows :

                          vector ( id = 1, fill = ''_START'' ); // Reset Handler

                           -->  vector ( id = 1, fill = ''Reset_Handler'' ); // Reset Handler

Best Regards,

Nouha