2015-11-11 11:08 AM
Hi,
I don't know why this code doesn't work. I have following simple code to check USART and the code is running on STM32F072 discovery board. But when I check PA2 pin with scope, it shows nothing. I also connect the board to PC serial port and check with hyperterminal and no luck. *******************************************static void USART_Config(void);
static void GPIO_Config(void); static void RCC_Config(void);/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program. * @param None * @retval None */ int main(void) { /* RCC configuration */ RCC_Config(); /* GPIO configuration */ GPIO_Config();/* USART configuration */
USART_Config();while(1)
{ while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData(USART2, 10);}
}/**
* @brief Configure the USART1 Device * @param None * @retval None */ static void USART_Config(void) { USART_InitTypeDef USART_InitStructure; /* USART1 configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - Two Stop Bit - Odd parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE); }/**
* @brief Configure the GPIO Device * @param None * @retval None */ static void GPIO_Config(void) { GPIO_InitTypeDef GPIO_InitStructure;/* Connect PXx to USART2_Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1);/* Connect PXx to USART2_Rx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1); /* Configure USART2 Tx/Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); }/**
* @brief Configure the RCC * @param None * @retval None */ static void RCC_Config(void) { RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); //enable GPIOA clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); //enable USART2 clock}
#rtfm2015-11-13 1:57 PM
/* Private function prototypes -----------------------------------------------*/
static void USART_Config(void); static void GPIO_Config(void); static void RCC_Config(void);/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program. * @param None * @retval None */ int main(void) { /* RCC configuration */ RCC_Config(); /* GPIO configuration */ GPIO_Config();/* USART configuration */
USART_Config();while(1)
{ while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 65); } }/**
* @brief Configure the USART1 Device * @param None * @retval None */ static void USART_Config(void) { USART_InitTypeDef USART_InitStructure; /* USART1 configured as follow: - BaudRate = 115200 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); }/**
* @brief Configure the GPIO Device * @param None * @retval None */ static void GPIO_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; /* Configure USART2 Tx/Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect PXx to USART1_Tx */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0);/* Connect PXx to USART1_Rx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0); // }/**
* @brief Configure the RCC * @param None * @retval None */ static void RCC_Config(void) { RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); //enable GPIOA clock // RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); //enable USART2 clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); //enable USART1 clock}
2015-11-13 3:22 PM
GPIO_AF_1 not 0
2015-11-13 4:02 PM
2015-11-13 5:46 PM
This works for me, signal out of PA9
/* Includes ------------------------------------------------------------------*/
#include ''stm32f072b_discovery.h''
/** @addtogroup STM32F0xx_DISCOVERY_Templates
* @{
*/
static void USART_Config(void);
static void GPIO_Config(void);
static void RCC_Config(void);
/**
* @brief Configure the USART1 Device
* @param None
* @retval None
*/
static void USART_Config(void)
{
USART_InitTypeDef USART_InitStructure;
/* USART1 configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- Two Stop Bit
- Odd parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
/**
* @brief Configure the GPIO Device
* @param None
* @retval None
*/
static void GPIO_Config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Configure USART1 Tx/Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect PXx to USART1_Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
/* Connect PXx to USART1_Rx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
}
/**
* @brief Configure the RCC
* @param None
* @retval None
*/
static void RCC_Config(void)
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); //enable GPIOA clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); //enable USART1 clock
}
/**
* @brief Main program.
* @param None
* @retval None
*/
int main(void)
{
/*!< At this stage the microcontroller clock setting is already configured,
this is done through SystemInit() function which is called from startup
file (startup_stm32f0xx.s) before to branch to application main.
To reconfigure the default setting of SystemInit() function, refer to
system_stm32f0xx.c file
*/
/* Add your application code here */
/* RCC configuration */
RCC_Config();
/* GPIO configuration */
GPIO_Config();
/* USART configuration */
USART_Config();
while(1)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
USART_SendData(USART1, 65);
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d
'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
2015-11-17 2:33 PM
I had a similar problem. The discovery board is set up as if the on-board debugger has virtul com on USART1. It does not. You will need to get out a soldering iron and change some solder bridges on the bottom side. As stated by the others above, this is a board you need to really carefully look at the board manual. Things are not as they seem.