2016-09-28 1:19 PM
Hello everybody,
since two days I struggle with curious noises at Pin 6 (TQFP32) by STM32F051K8. In my application I try to start TIM2 with TIM14 in kaskade mode (I have slight changed the sample code). I attach my source and screenshots with the signals. On the screen you can see signal of TIM14 (yellow) Pin 10 and signal with noises of TIM2 Pin 6 (blue). Has anyone any idea what's wrong? Thanks in advance! #stm32f051 #tim2 #tim142016-09-28 1:43 PM
and here is the source code ...
________________ Attachments : main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0tc&d=%2Fa%2F0X0000000bfD%2FXFcjL6TvyuaTPggATWSursNWj.wlmYrMa2XrdBgLIu4&asPdf=false2016-09-29 4:25 AM
Hi richter.andrey,
The TIM2_CH1 is on PA0 and not on PA6. Verify that you put the measure point on the right place , and GND is connected. Fothe code it seems ok , just checkth TIM2_CH1 pin polarity and delect the CtrlOutputEnable for TIM14.-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.