cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F050F6: 1or 2 USART?

johnlee
Associate II
Posted on November 18, 2013 at 00:11

The device selection says 2 USART, The datasheet says:

'1 x USART supporting master synchronous 

SPI and modem control; one with ISO7816 

interface, LIN, IrDA capability auto baud 

rate detection and wakeup feature'

But also says it only has 1 usart.  I am confused. Can I hook up 2 115200 8N1 devices concurrently or no? Id prefer not to make a software usart, but I really want the tssop20 package

Thank you

John
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on November 18, 2013 at 00:25

Other STM32F0xx parts have TWO USART, the part you selected has ONE.

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00065136.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
johnlee
Associate II
Posted on November 18, 2013 at 00:35

http://www.st.com/web/en/catalog/mmc/FM141/SC1169

Like I said, The device selection indicates it has 2 USARTS, and the datasheet is ambiguous?

Posted on November 18, 2013 at 02:02

The selector might indicate two, but the data sheet doesn't seem to be ambiguous about there being just one, and what pins that is available on. There are no references to USART2

Does Micro Xplorer suggest there are two?

How about the STM32F030? It has two, though not in the TSOP20

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN1826/PF258968

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00088500.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..