cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F050F4P6 - I2C slave error

kidteam
Associate
Posted on May 15, 2014 at 16:57

I am use STM32F050F4P6 as I2C slave device with address 0xC8

But it not work

When i send 0xC8 or 0xC9 from master, STM32F0 is not ack and not work

Please help me

code main.c

[CODE]

#include <stm32f0xx.h>

void Init(void);

void Interrupt_conf(void);

void I2C_Begin(void);

int main(void) {

Init();

Interrupt_conf();

I2C_Begin();

while(1) {

}

}

void Interrupt_conf(void) {

NVIC_InitTypeDef NVIC_InitStructure;

  

/* Reconfigure and enable I2C1 error interrupt to have the higher priority */

NVIC_InitStructure.NVIC_IRQChannel = I2C1_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

void Init(void) {

//khoi tao I2C

//===============================================================

GPIO_InitTypeDef  GPIO_InitStructure;

    I2C_InitTypeDef  I2C_InitStructure;

RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);

    // cho phep clock GPIOA

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

    /* I2C1 clock enable */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);

    /* I2C1 SDA and SCL configuration */

// SCL PA9

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

GPIO_Init(GPIOA, &GPIO_InitStructure);

I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Disable;

I2C_InitStructure.I2C_DigitalFilter = 0x00;

    I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

    I2C_InitStructure.I2C_OwnAddress1 = 0xC8;

    I2C_InitStructure.I2C_Timing = 0x00210507;

    I2C_Init(I2C1, &I2C_InitStructure);

I2C_Cmd(I2C1, ENABLE);

}

void I2C_Begin(void) {

/* Enable Event IT needed for ADDR and STOPF events ITs */

I2C1->CR1 |= I2C_CR1_ADDRIE ;

I2C1->CR1 |= I2C_CR1_STOPIE ;

/* Enable Error IT */

I2C1->CR1 |= I2C_CR1_ERRIE;

/* Enable Buffer IT (TXE and RXNE ITs) */

I2C1->CR1 |= I2C_CR1_TXIE;

I2C1->CR1 |= I2C_CR1_RXIE;

}

[/CODE]

code isr.c

[CODE]

#include <stm32f0xx.h>

uint8_t tmp;

uint16_t Tx_Idx1=0;

uint8_t Buffer_Rx[256];

uint8_t numOfSend;

uint8_t countOfSend;

uint8_t Buffer_Tx1[] = {

0x04, 0x11, 0x33, 0x43, \

0x23, 0xAB, 0x03, 0x4D, 0x9D, 0x47, 0xC6, 0x1F, 0xF1, 0x6D, 0x54, 0xA8, 0xF5, 0x75, 0x36, 0x9D, \

0x34, 0x9D, 0x24, 0xDE, 0xA2, 0x4A, 0x82, 0xA1, 0x04, 0x18, 0xD4, 0x19, 0x4C, 0xC2, 0xF3, 0x5E, \

0xCE, 0x24, 0xB6, \

0x23, 0x5D, 0x5B, 0x41, 0xBF, 0x5A, 0x2A, 0x95, 0x75, 0x0A, 0xD5, 0xF5, 0x34, 0xAB, 0xDE, 0x90, \

0x48, 0xFE, 0x28, 0xF9, 0xEC, 0x9C, 0x49, 0xCE, 0x3A, 0x0F, 0xB7, 0xCD, 0x1A, 0xE7, 0x88, 0xF1, \

0x53, 0xED, 0x2B, \

0x04, 0x00, 0x03, 0x40, \

0x04, 0x00, 0x03, 0x40, \

0x04, 0x11, 0x33, 0x43, \

0x04, 0x00, 0x03, 0x40, \

0x04, 0x11, 0x33, 0x43, \

0x04, 0x00, 0x03, 0x40, \

0x04, 0x00, 0x03, 0x40, \

0x04, 0x11, 0x33, 0x43, \

0x04, 0x00, 0x03, 0x40, \

0x23, 0x3F, 0x09, 0x75, 0x39, 0xC9, 0x10, 0x84, 0x7D, 0x4D, 0x24, 0x1C, 0xF2, 0x1F, 0xD5, 0xF4, \

0xEE, 0xAB, 0x1F, 0x1B, 0xAE, 0x21, 0x4F, 0x4B, 0x65, 0x10, 0xF6, 0x16, 0xF1, 0x94, 0x5A, 0x99, \

0xC7, 0xB5, 0x05, \

0x04, 0x11, 0x33, 0x43, \

0x23, 0xAD, 0xB3, 0xE6, 0x97, 0x58, 0x2C, 0x88, 0x9D, 0x7C, 0x44, 0x7A, 0x6C, 0xC0, 0xBF, 0x11, \

0x5D, 0xD4, 0x9A, 0x9A, 0x58, 0x80, 0xB2, 0xE8, 0xAF, 0x56, 0xB6, 0xA7, 0x09, 0xB4, 0x43, 0x33, \

0x3D, 0xA3, 0x3A, \

0x04, 0x00, 0x03, 0x40, \

0x23, 0x5E, 0x06, 0xB3, 0x48, 0x76, 0xB0, 0x60, 0x71, 0x27, 0x8F, 0xFC, 0x00, 0x62, 0x23, 0xBB, \

0x69, 0x92, 0x19, 0x9F, 0x4A, 0xF2, 0xF0, 0x23, 0x21, 0xEC, 0x81, 0x45, 0x98, 0xA6, 0x3D, 0xD4, \

0x6C, 0x7E, 0x90

};

//ham ngat I2C1

void I2C1_IRQHandler(void) {

//ham ngat I2C1

//kiem tra xem cai gi gay ra ngat

uint32_t isr;

isr=I2C1->ISR;

//kiem tra xem co trong che do SLAVE khong

//ADDRESS matched

if(isr&I2C_ISR_ADDR) {

//kiem tra chieu truyen du lieu

if(isr&I2C_ISR_DIR) {

//chieu truyen du lieu

//slave truyen du lieu

numOfSend=Buffer_Tx1[Tx_Idx1];

countOfSend=0;

} else {

//slave nhan du lieu

//=======================

}

isr=0;

}

if(isr & I2C_ISR_TXE) {

++countOfSend;

if(countOfSend>numOfSend) {

//==================================================================

I2C1->TXDR = 0xFF;

} else {

tmp=Buffer_Tx1[Tx_Idx1++];

I2C1->TXDR = tmp;

//==================================================================

}

isr=0;

}

if(isr & I2C_ISR_RXNE) {

tmp=I2C1->RXDR;

isr=0;

}

if(isr & I2C_ISR_STOPF) {

I2C1->CR1=I2C_CR1_PE;

isr=0;

}

//kiem tra loi

if(isr & I2C_ISR_ARLO) {

I2C1->ICR |= I2C_ICR_ARLOCF;

isr=0;

}

if(isr & I2C_ISR_BERR) {

I2C1->ICR |= I2C_ICR_BERRCF;

isr=0;

}

if(isr & I2C_ISR_OVR) {

I2C1->ICR |= I2C_ICR_OVRCF;

isr=0;

}

}

[/CODE]
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0