STM32F042F6- TSSOP20- Where is the TIMER 2 Channel 1?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-01 9:28 AM
Posted on November 01, 2016 at 17:28
Dear all experts,
I am programming Incremental Encoder Reading project for 2 encoders.I intend to use TIM2, and TIM3 for Encoder Config with 4X Reading. I check the datasheet (DM00105814) for MCU Pin configuration.For TIM3, I can see TIM3-CH1, and TIM3_CH2 are Pin PA6, PA7For TIM2, I cannot find TIM2-CH1, instead of that, I see 2 pin PA0 and PA5 can config to same function TIM2-CH1-ETR.As subject, Could any one can help me to find out TIM2-CH1?Thank you in advance.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-01 9:39 AM
Posted on November 01, 2016 at 17:39
TIM2-CH1-ETR is TIM2-CH1 and TIM2-ETR, as ETR is an input only it doesn't conflict, and would need to be configured inside the timer to be used.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-01 10:08 AM
Posted on November 01, 2016 at 18:08
Thank you very much Clive1,
I solved the problem by :/* (3) Select AF2 on PA5 in AFRL for TIM2_CH1 */
GPIOA
->
AFR
[
0
] |=
0x02
<< (
5
*
4
);
/* (3) */