cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042C6 SPI2 RXNE clears before reading DR

EmbedMaster
Associate II
Posted on June 24, 2016 at 09:04

Good day!

I have simple SPI read func:

bool SPIRead(byte reg, byte &result)
{
ushort timeoff=0x100;
volatile short temp;
temp=SPI2->DR;// To clear DR
temp=SPI2->DR;
temp=SPI2->DR;
CS_EN;// i still don't understand why ST can't do this in hardware mode.

SPI2->DR=reg|0x80;
busy=true;
while(!(SPI2->SR&SPI_SR_RXNE) && timeoff--);
CS_DIS;
result=SPI2->DR>>8;
busy=false;
return timeoff > 0;
}

This func is called for 50 times per sec (SPI clock = 93750Hz (24MHz AP1B clock/256) ). I have next problem - when i debug this code (in keil), when i step

SPI2->DR=reg|0x80;

i see in regs FRLVL=2 and RXNE = 1. This is normal - there was 16 clocks and mcu received 16 bits. But in next step (busy = true;) in asm (movs r0,#0x01) FRLVL cleared and RXNE cleared too. They cleared before i read DR. The datasheet says that: A read access to the SPIx_DR register must be managed by the RXNE event. This event is triggered when data is stored in RXFIFO and the threshold (defined by FRXTH bit) is reached. When RXNE is cleared, RXFIFO is considered to be empty. Ie RXNE

bit must

not be cleared

until I

read

register

. It is not mentioned in errata. What i am doing wrong? Thanks!
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
EmbedMaster
Associate II
Posted on June 24, 2016 at 09:13

Posted on June 24, 2016 at 09:38

It is not mentioned in errata. What i am doing wrong?

You are reading it in the debugger, it doesn't have magical access to the registers, and alters the status. Probe the peripheral with your own code, don't place a peripheral view over it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..