cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F031 SPI Slave can not send out CRC Correctly

Wang Jun
Associate
Posted on March 02, 2018 at 09:52

STM32F031  is configurated as SPI Slave, CRC result can not be send out correctly. Attached the whole project. 

I also designed one SPI master by another STM32F031 for this testing. The waveform that master sent is right.

MxCube Initial code:

  SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;

  SPI_InitStruct.Mode = LL_SPI_MODE_SLAVE;

  SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_16BIT;

  SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_Low;

  SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;

  SPI_InitStruct.NSS = LL_SPI_NSS_HARD_INPUT;

 SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV128;

  SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;

  SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_ENABLE;

  SPI_InitStruct.CRCPoly = 0x1021;

  LL_SPI_Init(SPI1, &SPI_InitStruct);

  LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);

  LL_SPI_SetCRCWidth(SPI1, LL_SPI_CRC_16BIT);

  LL_SPI_DisableNSSPulseMgt(SPI1);

Send data and Enable CRCNext in Main function.

   for(TxCnt=3;TxCnt<11;TxCnt++)

   {

    while(LL_SPI_GetTxFIFOLevel(SPI1)==LL_SPI_TX_FIFO_FULL);

    LL_SPI_TransmitData16(SPI1,TxCnt);

    if(TxCnt==10)

    {

     while(LL_SPI_GetTxFIFOLevel(SPI1)!=LL_SPI_TX_FIFO_EMPTY);

     i=LL_SPI_GetTxCRC(SPI1);

     LL_SPI_SetCRCNext(SPI1);

    }

   }
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0