cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030F4P6 TSSOP20 OSC32

MBelk
Associate II

There isn't any PC14 PC15. Is it really inaxessible on this MCU and I'm have to find suitable HSE crystal in order to get high-presition RTC?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
moatjon
Associate III

Hello MBelk,

Pins PC14 and PC15 are indeed not present on the TSSOP20 version of the STM32F030. As such, you cannot add an external low-speed oscillator. You can still use the internal low-speed clock (LSI) as a source for the RTC, although the achieved accuracy won't be as high as when using an external low-speed clock.

View solution in original post

2 REPLIES 2
moatjon
Associate III

Hello MBelk,

Pins PC14 and PC15 are indeed not present on the TSSOP20 version of the STM32F030. As such, you cannot add an external low-speed oscillator. You can still use the internal low-speed clock (LSI) as a source for the RTC, although the achieved accuracy won't be as high as when using an external low-speed clock.

Yes, but 4.096 MHs standard HSE crystal resonator will helps.