cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030F4 and STM32F103C4Tx CHİP BOOT

bngstskn
Associate III

I use the STM32F103C4 and STM32F030F4 chip. I design a card with these chips. How I can programmable these chips? If I add SWDIO, SWCLK, +3.3V, and GND pins to the card as a male header, Can I connect the ST-LINK v3 to these pins and program it directly? I added a photo of the design diagram. Or should I add boot0 and boot1 pins like on the STM32F103 card?

bngstskn_0-1695802112856.pngbngstskn_1-1695802143447.png

First photo ----- STM32F0

Second photo -------STM32F1

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @bngstskn 

In such a case, is always better to follow the same configuration of a board based on this MCU.

Best regards.

II

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @bngstskn 

In such a case, is always better to follow the same configuration of a board based on this MCU.

Best regards.

II

I added the necessary boot0 and boot1 pins by looking at the boards of both MCUs.  And I added reset pin.Thank you for the recommendation. I hope it works smoothly

bngstskn_0-1695804825911.png

bngstskn_1-1695804857488.png