cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0308-DISCOVERY I2C Configuration

vendor
Associate II
Posted on February 12, 2014 at 20:22

My original post *poof* gone..

I am attempting to use I2C2, however Oscilliscope does not see any activity on either SCL or SDA. Using STM32F0308-Discovery. Obviously timing parameter is wrong, have tried many as I seem to be missing documentation, not sure that is only issue here. I have been wrestling with this issue for 2+ weeks and have exhausted all other options, Any assistance would be greatly appreciated. Note I am using GPIO PF6/PF7 as I2C2, as this part does not support I2C1 for these pins,  I2C1 is unused. Both pins are high at power up with external pull up resistors.  Have start delay of 50ms after reset and  prior to initializing I2C2.

void print7SegDisplay(void) {

  uint16_t i =0;

  uint16_t testdata = 0x7D;

  

  // Configures the slave address to be transmitted after start generation.

  I2C_SlaveAddressConfig(I2C2, 0x70);

  I2C_MasterRequestConfig(I2C2, I2C_Direction_Transmitter);

  I2C_GenerateSTART(I2C2, ENABLE);

  I2C_NumberOfBytesConfig(I2C2, 9); // number of bytes to send

  I2C_SendData(I2C2, 0x21);  // turn on Oscillator

  I2C_SendData(I2C2, 0x81);  // turn on Display

  

  for (i=0; i<8; i++) {

    I2C_SendData(I2C2, testdata);

    I2C_SendData(I2C2, testdata >> 8);    

  }

  I2C_GenerateSTOP(I2C2, ENABLE); 

 

}

void I2C_Configure(void)

{

  // I2C2 Configuration STM32F0308-DISCOVERY on GPIO PF6 & PF7 

  // Note does not use I2C1 

  // 

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);

  

  GPIO_InitTypeDef GPIO_InitStructure;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 ; //SCL 

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_PinAFConfig(GPIOF, GPIO_PinSource6, GPIO_AF_1); 

  GPIO_Init(GPIOF, &GPIO_InitStructure); 

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 ; //SDA

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

  GPIO_PinAFConfig(GPIOF, GPIO_PinSource7, GPIO_AF_1); 

  GPIO_Init(GPIOF, &GPIO_InitStructure); 

  

  // I2C_InitTypeDef  I2C_InitStructure;

  I2C_InitTypeDef I2C_InitStructure; 

  

  I2C_InitStructure.I2C_Timing              = 0x00;

  I2C_InitStructure.I2C_AnalogFilter        = I2C_AnalogFilter_Disable;

  I2C_InitStructure.I2C_DigitalFilter       = 0x00;

  I2C_InitStructure.I2C_Mode                = I2C_Mode_I2C; 

  I2C_InitStructure.I2C_OwnAddress1         = 0x00;

  I2C_InitStructure.I2C_Ack                 = I2C_Ack_Enable;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

     

  I2C_Cmd(I2C2, ENABLE);//I2C Peripheral Enable 

  I2C_Init(I2C2, &I2C_InitStructure);//Apply I2C configuration after enabling it    

}

 

#stm32f03 #discovery #i2c
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 12, 2014 at 20:56

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // Definitely needs to be OD

Pretty sure you can't just jamb I2C functions one after another, you'd need to spin waiting for status/state changes, TXE, etc.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
vendor
Associate II
Posted on February 12, 2014 at 21:47

Clive,

Again, thank you. I made change to OD, still no acitvity on either SDA or SCL. I am having trouble determining  value for this statement: 

I2C_InitStructure.I2C_Timing              = 0x00; 

Pretty sure this is incorrect.. but cannot find any reference to the correct value other than a very cryptic  '' uint32_t I2C_Timing;              /*!< Specifies the I2C_TIMINGR_register value.

                                         This parameter must be set by referring to I2C_Timing_Config_Tool*/''    

This appears to be missing from the toolset (and I have looked everywhere). 

In regards to the writing to the I2C, I know that is wrong, I just wanted to hit the I2C bus with some data looking for a heartbeat, or at least a single pulse of data. Just trying to properly initialize I2C2 for now. 

I thank you in advance for your assistance.

 

Rick43065