cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030 UART problem

Posted on September 28, 2017 at 17:58

Hi all,

I'm trying to send an HTTP message through Ethernet interface using a WIFI external device. For this, I use HAL_UART functions as shown:

HAL_UART_Transmit(huart, messageTX,lengthOfmessage, timeoutTX);

UART has the following configuration:

static void MX_USART1_UART_Init(void)

{

huart1.Instance = USART1;

huart1.Init.BaudRate = 115200;

huart1.Init.WordLength = UART_WORDLENGTH_8B;

huart1.Init.StopBits = UART_STOPBITS_1;

huart1.Init.Parity = UART_PARITY_NONE;

huart1.Init.Mode = UART_MODE_TX_RX;

huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart1.Init.OverSampling = UART_OVERSAMPLING_16;

huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

if (HAL_UART_Init(&huart1) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

}

My tests results was (monitoring with Wireshark software):

1) Set the parameters as follows:

- messageTX = 'GET /registro/index.php/?solicitud=Hello HTTP/1.1\ \r\n Host:192.168.1.116\r\n\r\n'

lengthOfmessage = 75

- timeoutTX = 100

 

Results are OK, messageTX is successfully sent

2) Set the parameters as follows:

- messageTX = GET /registro/index.php/?solicitud=<horfeus><firma><IP>192.168.1.160</IP><TipoCliente>4</TipoCliente><tiempo>23/01/2017-04:57:04</tiempo><edificio>53</edificio><TipoAula>6</TipoAula><aula>MA21FPLA1</aula><serie>00352738</serie></firma></horfeus> <horfeus><firma><IP>192.168.1.160</IP><TipoCliente>4</TipoCliente><tiempo>23/01/2017-04:57:04</tiempo><edificio>53</edificio><TipoAula>6</TipoAula><aula>MA21FPLA1</aula><serie>00352738</serie></firma></horfeus> HTTP/1.1\ \r\n Host:192.168.1.116\r\n\r\n'

lengthOfmessage = 275

- timeoutTX = 100

Here, results are NOK, messageTX is not successfully sent. In Wireshark SW I receive a message with size 19 bytes. I think this size 19 indicates the size that exceeds my messageTX, i.e.:

messageTX(275 bytes) - messageReceived(19 bytes) = 256 bytes

So, it's possible that STM32f030 UART interface limits my messageTX size in 256 bytes?

 

Please, help me.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on September 28, 2017 at 18:22

Hello!

through Ethernet interface using a WIFI external device.

UART is capable to send more than 256 Bytes by calling HAL_UART_Transmit(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout). (Also IT Versions)

Is WiFi external device capable to handle more than  256 Bytes?

Check also the definition of 'message_length' in your code if it has 8bit width.

Regards

vf

View solution in original post

3 REPLIES 3
Posted on September 28, 2017 at 18:22

Hello!

through Ethernet interface using a WIFI external device.

UART is capable to send more than 256 Bytes by calling HAL_UART_Transmit(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout). (Also IT Versions)

Is WiFi external device capable to handle more than  256 Bytes?

Check also the definition of 'message_length' in your code if it has 8bit width.

Regards

vf

Posted on September 28, 2017 at 18:22

>>So, it's possible that STM32f030 UART interface limits my message TX size in 256 bytes?

It is improbable, the USART one has a single byte holding register. Transmission would be limited by the data you provide, and the realistic transmission time for that data vs timeout.

Does your device require flow control?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 02, 2017 at 19:16

Yes! Problem was in lengthOfmessage definition (uint8_t in my case).

Thanks for your suppor! =)