STM32CubeMX, FatFS and SDIO?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-20 1:57 PM
Everyone,
How can I use cubeMX for SDcard ? I have generated for MDK but :
this function doesn't work , from UM1721
User manualDeveloping Applications on STM32Cube with FatFs page 21.:
uint32_t wbytes; /* File write counts */
uint8_t wtext[] = 'text to write logical disk'; /* File write buffer */if(FATFS_LinkDriver(&mynewdisk_Driver, mynewdiskPath) == 0){if(f_mount(&mynewdiskFatFs, (TCHAR const*)mynewdiskPath, 0) == FR_OK){if(f_open(&MyFile, 'STM32.TXT', FA_CREATE_ALWAYS | FA_WRITE) == FR_OK){if(f_write(&MyFile, wtext, sizeof(wtext), (void *)&wbytes) == FR_OK);{f_close(&MyFile);}}}}FATFS_UnLinkDriver(mynewdiskPath);This variable :
&mynewdisk_Driver doesn't exist, which file is related ?
Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 7:32 PM
You should be able to enable pull-ups on the pins internally.
The FatFs code will not work if the underlying SDIO code isn't functional.
What pin is being used on the socket's card detect?
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
‎2017-04-26 7:33 PM
Lower the SDIO init speed, there's one file for doing that. I have
posted in here I reckon.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 7:34 PM
That's right, connect SD Detect as well, it's inside the code PB14 if
I'm not wrong..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 8:06 PM
Yeah, in STM32CubeMX under 'Configuration' -> 'GPIO' a 'Pin Configuration' window comes up. Under the 'SDIO' tab it shows the SDIO pins, which are defaulted as 'Alternate Function Push Pull' for 'GPIO mode', but under 'GPIO Pull-up/Pull-down' it's defaulted as 'No pull-up and no pull down' - I can change this to 'Pull-up' for just the 4 data lines and the CMD line only (so no open-drain external pull-up resistors needed - just internal). By default STM32Cube SDIO settings don't include the SD detect pin; I'll have to do that manually. I'll change the clock speed setting to what you put manually in code; but I'll have to see what this changes in the clock tree as well.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 9:52 PM
Yes it depends on the main clock from HSE or HSI or internal and divider,
I'm not in windows now so I can not run STM32CubeMX but I'll have a look
on my code, there're some hints on it..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 10:05 PM
Have a dig on the code at stm32f1xx_II_sdmmc.h ==> STM32F103, for
STM32F4xx, I reckon you need to change the name.
/* SDIO Intialization Frequency (400KHz max) */ ==> check your main
clock and divider on STM32CubeMX
&sharpdefine SDIO_INIT_CLK_DIV ((uint8_t)0xC3)
/* SDIO Data Transfer Frequency */
/* SDIO_CK = SDIOCLK / (SDIO_TRANSFER_CLK_DIV + 2) */
&sharpdefine SDIO_TRANSFER_CLK_DIV ((uint8_t)0x0F) // ==72/(15+2) = 4.23MHz
, work best for my MP3 chip syncronization speed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 10:22 PM
Some debug to UART for seeing the response
/=====/
/**
@brief Initializes the SD card device.
@retval SD status
*/
uint8_t BSP_SD_Init(void)
{
uint8_t sd_state = MSD_OK;
printf('BSP_SD_Init Function!\n');
/* Check if the SD card is plugged in the slot */
if (BSP_SD_IsDetected() != SD_PRESENT)
{
return MSD_ERROR;
}
/* HAL SD initialization */
sd_state = HAL_SD_Init(&hsd, &SDCardInfo);
&sharpifdef BUS_4BITS
/* Configure SD Bus width */
if (sd_state == MSD_OK)
{
/* Enable wide operation */
if (HAL_SD_WideBusOperation_Config(&hsd, SDIO_BUS_WIDE_4B) != SD_OK)
{
sd_state = MSD_ERROR;
printf('MSD_ERROR\n');
}
else
{
sd_state = MSD_OK;
printf('MSD_OK \n');
}
}
&sharpendif
return sd_state;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-26 10:23 PM
&sharpdefine __SD_DETECT_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-27 1:19 PM
I have
__HAL_RCC_GPIOB_CLK_ENABLE() defined and enabling the clock on that port. Are you redefining this function
__SD_DETECT_GPIO_CLK_ENABLE() ? I don't have __SD_DETECT_GPIO_CLK_ENABLE() in my code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-27 1:29 PM
This is the list of alternate functions for PB14 in CubeMX. Which one would be the Card Detect for SDIO mode? How would you write this in the code?