cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX and HAL Drivers poor documentation

astrid
Associate II
Posted on November 02, 2015 at 19:32

I acquainted with STM32CubeMX amd HAL Drivers for STM32F1, but I'm really some confused.For example SPI in HAL Drivers User Manual I find function HAL_SPI_Transmit()The thirdy parameters is TimeoutDocumentation say Timeout is Timeout duration , of what? Why and how OK I loot in function definition in line 400 of the xxxxx_SPI.cTimeout is used as parametrs in function  SPI_WaitOnFlagUntilTimeout()Unfortunately, the documentation again say Timout duration and on line 2286 is Timout compared with HAL_MAX_DE''AY.What is HAL_MAX_DELAY I could find so far.Documentation is a bad joke.Is there any better documentation and examples described above function parameters?Rr how you can become familiar with the HAL layer Drivers?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 03, 2015 at 10:29

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32CubeMX%20Hall%20Driver%20%2c%20documentation&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=12]cross post