cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.8.0 Bug: SPI Baud Prescaler (Fixed)

james2399
Associate II
Posted on June 16, 2015 at 03:49

(I managed to fix this as I was writing this post)

STM32CubeMX 4.8.0 was generating the incorrect prescaler value for SPI3 after upgrading. .ioc contained:

SPI3.BaudRatePrescaler=SPI_BAUDRATEPRESCALER_8
SPI3.BaudRatePrescaler-Full_Duplex_Master=SPI_BAUDRATEPRESCALER_32
SPI3.CalculateBaudRate=3.0 MBits/s
SPI3.CalculateBaudRate-Full_Duplex_Master=1.3125 MBits/s
SPI3.IPParameters=BaudRatePrescaler-Full_Duplex_Master,TIMode-Full_Duplex_Master,Mode-Full_Duplex_Master,CalculateBaudRate-Full_Duplex_Master,BaudRatePrescaler,NSS-Full_Duplex_Master,Mode,CalculateBaudRate
SPI3.Mode=SPI_MODE_MASTER
SPI3.Mode-Full_Duplex_Master=SPI_MODE_MASTER
SPI3.NSS-Full_Duplex_Master=SPI_NSS_SOFT
SPI3.TIMode-Full_Duplex_Master=SPI_TIMODE_DISABLED

main.c was generating:

hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;

The SPI3 Configuration dialog is showing: Prescaler: 8 Baud Rate: 3.0 MBits/s The fix was to manually delete the SPI3 configuration lines containing ''-Full_Duplex_Master'' and reload the .ioc The I2S configuration contained similar duplications, but didn't cause any code generation problems.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0