STM32CubeMX 4.7.0 issue? Can't configure I2C 400KHz fast mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-04-09 6:54 AM
Posted on April 09, 2015 at 15:54
Hi,
after upgrading to CubeMX 4.7.0 I can no longer configure I2C to 400KHz. I can select Fast Mode but the only valid range is still 0-100000 Hz. I also made sure that my PCLK1 is a multiple of 10. This is on an STM32F401RCTx for example.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0