cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubemx 4.15.0 : incorrect board file for nucleoF746

alexandre23
Associate III
Posted on June 09, 2016 at 10:34

Hello, selecting nucleoF746 in cubemx (in the nucleo 144 line), i can see somme errors :

1/ the HSE frequency is 8mhz and not 16Mhz, and the clock in not corre ct (RCC not enabled, prescaler not set)

2/ pin PB00 LD1_Green is missing

A fixed .iocis attached to this post.

#nucleo-f746g-stm32cubemx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Walid FTITI_O
Senior II
Posted on June 09, 2016 at 11:23

Hi bustico.alexandre,

Thanks for the feedback. I report this internally to our CubeMx team.

(just for the RCC, the HSE will be selected in the clock tree when it is enabled by user in the RCC peripheral)

-Hannibal-

Jeanne Joly
Senior III
Posted on November 08, 2016 at 10:57

Hello bustico.alexandre,

Thank you for reporting the bug you saw.

We modified some iocs to solve the issue you highlighted.

The modifications are added in CubeMX4.18.

BR

Eric Dampierre