2025-12-22 9:41 PM
1. Please suggest the pin for programming interface or documents
2. Programme example for tick timer, two external interrupts? library
2025-12-23 12:10 AM - edited 2025-12-23 12:15 AM
My copilot said:
Even in the 8‑pin SOIC package, the STM32C011J4M6 exposes the full SWD interface.
| SWDIO | PA13 | Bidirectional debug data |
| SWCLK | PA14 | Debug clock |
| NRST | PA0 | Optional but strongly recommended |
| VDD / VSS | — | Power + ground |
These are the same pins used on all STM32C0 devices.
You’ll want these three documents from ST:
Datasheet (STM32C011x4/x6)
Reference Manual (RM0490 — STM32C0 series)
Errata Sheet (always worth checking)
You can find them on ST’s product page by searching “STM32C011J4M6”.
Below is a clean, minimal, reproducible example using HAL. It demonstrates:
SysTick running at 1 ms
Two EXTI lines on PA1 and PA2
Interrupt handlers toggling flags
No CubeMX required
... (code snippets and explanations follow)
Notes:
- the toolchain was recently upgraded to STM32Cube for VS Code - STMicroelectronics
and many existing tutorials... dont reflect that yet,
- try the STM32 Sidekick (chat button down right corner)
hth
KnarfB