Question
stm32c011
please let me know my coding is correct ,whether usage of my exti is correct
while (1)
{
HAL_Delay(300);
// MAINS INPUT
Adc_Mains();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Mains=HAL_ADC_GetValue(&hadc1);
Mains=Mains*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//Battery operation
Adc_Vbat();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Vbat=HAL_ADC_GetValue(&hadc1);
Vbat=Vbat*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//OPEN CIRCUIT DETECT
Adc_OCD();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
OCD=HAL_ADC_GetValue(&hadc1);
OCD=OCD*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
//BATTERY TEMPARATURE
Adc_Temp();
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
Temp=HAL_ADC_GetValue(&hadc1);
Temp=Temp*2/4095;
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
// Check mains and mains fail
if(Mains>0.1)
{
if((Mains<1) &&(Vbat>0.9))
{
En_Emergency(1);
Set_LED(0);
}
else
{
En_Emergency(0);
}
mainsOffTimer = 0;
}
// MAINS ON
if(Mains>1.2)
{
if(Vbat>1.5 || Vbat<0.5) //OPEN CIRCUIT OR ZERO BATT LEVEL
{
Set_LED(0);
Batt_Chrge(1);
}
else if(Vbat <0.94 ) // START CHARGING LEVEL
{
Set_LED(1);
Batt_Chrge(1);
}
else if(Vbat >0.98 ) // STOP CHARGING LEVEL
{
Set_LED(1);
Batt_Chrge(0);
}
//BATTERY TEMPARATURE CHECK
if(Temp<0.17 || Temp>0.83)
{
Batt_Chrge(0);
Triple_Flash();
}
else if((Temp>0.17 || Temp<0.83))
{
Batt_Chrge(1);
}
}
if(Mains<0.1)
{
mainsOffTimer++;
// Enter Shutdown mode if mains is off for 30 seconds
if (mainsOffTimer >= 300)
{
// Shutdown mode
// Disable EXTI for PA2 to prevent immediate wake-up
HAL_NVIC_DisableIRQ(EXTI2_3_IRQn);
// Enter deep sleep mode
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
__WFI();
// Re-enable EXTI for PA2 after wake-up
HAL_NVIC_EnableIRQ(EXTI2_3_IRQn);
}
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
*
*
*
**
*
**
**
**
**
*
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, EMERGENCY_Pin|LED_Pin|BATTCHRG_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : PA2 */
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : EMERGENCY_Pin LED_Pin BATTCHRG_Pin */
GPIO_InitStruct.Pin = EMERGENCY_Pin|LED_Pin|BATTCHRG_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI2_3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI2_3_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */