Skip to main content
Associate III
August 3, 2023
Question

Pwr_wakeup

  • August 3, 2023
  • 2 replies
  • 858 views

I couldn't able wakeup the system after standby (wakeup should be switching ON mains ) the wakeup pin PA2 is connected to mains pin configured for pwr wakeup.

 

 

int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */

 /* Enable Power Control clock */
 __HAL_RCC_PWR_CLK_ENABLE();
 /* Check if the system was resumed from Standby mode */
 if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
 {
 /* Clear Standby flag */
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
 /* Check and Clear the Wakeup flag */
 if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF4) != RESET)
 {
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF4);
 }
 }


 while(Mains<0.1)
 {
 	count++;
 	if(count>=30)
 	{
 		 HAL_PWR_EnterSTANDBYMode();

 	}
 	else
 	{
 		count=0;
 	}
 }
 HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_HIGH);




 while (1)
 {
	 HAL_Delay(100);
	 	 // MAINS INPUT
	 	 	 Adc_Mains();
	 	 	 HAL_ADC_Start(&hadc1);
	 	 	 HAL_ADC_PollForConversion(&hadc1,1000);
	 	 	 Mains=HAL_ADC_GetValue(&hadc1);
	 	 	 Mains=Mains*2/4095;
	 	 	 HAL_ADC_Stop(&hadc1);
	 HAL_Delay(100);

	 //Battery operation
	 Adc_Vbat();
	 HAL_ADC_Start(&hadc1);
	 HAL_ADC_PollForConversion(&hadc1,1000);
	 Vbat=HAL_ADC_GetValue(&hadc1);
	 Vbat=Vbat*2/4095;
	 HAL_ADC_Stop(&hadc1);
	 HAL_Delay(100);

	 //OPEN CIRCUIT DETECT
	 Adc_OCD();
	 	 	HAL_ADC_Start(&hadc1);
	 	 HAL_ADC_PollForConversion(&hadc1,1000);
	 	 OCD=HAL_ADC_GetValue(&hadc1);
	 	 OCD=OCD*2/4095;
	 	 HAL_ADC_Stop(&hadc1);
	 	 HAL_Delay(100);
	 	 //BATTERY TEMPARATURE
	 	 		Adc_Temp();
	 	 	 	 	HAL_ADC_Start(&hadc1);
	 	 	 	 HAL_ADC_PollForConversion(&hadc1,1000);
	 	 	 	 Temp=HAL_ADC_GetValue(&hadc1);
	 	 	 	 Temp=Temp*2/4095;
	 	 	 	 HAL_ADC_Stop(&hadc1);
	 	 	 	 HAL_Delay(100);

	 	 	 	// Check mains and mains fail

	 	 	 	if(Mains>0.1)


	 	 	 	{
	 	 	 		 if((Mains<1) &&(Vbat>0.9))
	 	 	 		 	 {
	 	 	 			 	 En_Emergency(1);
	 	 	 			 	Set_LED(0);

	 	 	 		 	 }

	 	 	 		 else
	 	 	 		 	 {
	 	 	 			 En_Emergency(0);
	 	 	 		 	 }

	 	 	 	}
	 	 	// MAINS ON
	 	 	if(Mains>1.2)
	 	 	{
	 	 		if(Vbat>1.5 || Vbat<0.5) //OPEN CIRCUIT OR ZERO BATT LEVEL
	 	 				{
	 	 				Set_LED(0);
	 	 				Batt_Chrge(1);
	 	 				}
	 	 		else if(Vbat <0.94 ) // START CHARGING LEVEL
	 	 				{
	 	 				Set_LED(1);
	 	 				Batt_Chrge(1);
	 	 				}
	 	 		else if(Vbat >0.98 ) // STOP CHARGING LEVEL
	 	 				{
	 	 				Set_LED(1);
	 	 				Batt_Chrge(0);

	 	 				}
	 	 		//BATTERY TEMPARATURE CHECK

	 	 	 if(Temp<0.17 || Temp>0.83)
	 	 	 {
	 	 		Batt_Chrge(0);
	 	 		Triple_Flash();
	 	 	 }
	 	 	 else if((Temp>0.17 || Temp<0.83))
	 	 	 {
	 	 		Batt_Chrge(1);

	 	 	 }
	 	 	}

 

 

This topic has been closed for replies.

2 replies

TDK
August 3, 2023

If Mains is initialized to 0, which as a global variable presumably it is, your code will never get out of this loop and thus will never enter the main loop.

 

 

 while(Mains<0.1)
 {
 	count++;
 	if(count>=30)
 	{
 		 HAL_PWR_EnterSTANDBYMode();

 	}
 	else
 	{
 		count=0;
 	}
 }

 

 

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
SRAM.11Author
Associate III
August 3, 2023

can you please help me to solve.

if(Mains<1)
{
count++;
if(count>=300);
{
HAL_PWREx_EnterSHUTDOWNMode();
}
}

i tried this too but the problem is in wakeup