STM324x9I-EVAL SPI port available?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-16 9:45 AM
Posted on January 16, 2015 at 18:45
When running STM32CubeMX and selecting this board it shows all SPI ports as unavailable (red X) except for SPI4 which has very limited functionality.
Am I interpreting this correctly? There is no way I can use any of the other SPI ports? (Even when not using some of the other peripherals?)Thanks!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-16 10:51 AM
Posted on January 16, 2015 at 19:51
I'd trust Cube (or MicroXplorer) to figure the pin conflicts more efficiently than I can do it with a pen and paper. You'd have to figure out where the conflicts are arising, and back out those associations.
Full featured boards like the STM324x9I-EVAL are there to demonstrate the function of already attached peripherals/hardware. Pins are already over subscribed to the point it has an I2C base IO Expander for some of the lower bandwidth IO/IRQ functions. Perhaps you need to have a more break-out level board, the STM32F429I-DISCO is not a good one, but seem to think WaveShare had a more open/plug-n-play type approach.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..