cancel
Showing results for 
Search instead for 
Did you mean: 

STM32429I-EVAL demonstration software available ?

John F.
Senior
Posted on November 20, 2013 at 10:07

Is the STM32429I-EVAL demonstration

software available on the ST website please?
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Amel NASRI
ST Employee
Posted on November 26, 2013 at 11:32

Hello John,

The firmware is not yet available in the web, it is coming soon even though it was anticipated in the user manual.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

John F.
Senior
Posted on November 26, 2013 at 13:20

Hi Mayla,

Thanks for your reply. I'll wait for the firmware to arrive. Also ... can we expect the STM32F429 larger packages LQFP 208 and TFBGA 216 any time soon?

mmiu
Associate
Posted on December 11, 2013 at 23:29

Mayla,

Since you mentioned the User Manual, will there be additional documentation that includes a memory map for the STM32429I-EVAL1 board? For example, I found a memory map for the STM3240G eval board in it's Programming Manual.

Thanks,

Michael

Posted on December 12, 2013 at 05:24

It's not that complicated to figure out

0x08000000 FLASH 2MB
0x10000000 CCM 64KB
0x20000000 SRAM Int 192KB
0x40024000 NVRAM 4KB
0x60000000 NOR 16MB
0x64000000 SRAM Ext 2MB
0xC0000000 SDRAM 8MB

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gene23
Associate II
Posted on January 08, 2014 at 17:15

I am also very interested in the demonstration software. First of all, I was trying different code on the Eval board, so I erased the demo software. Second of all, the demo software has code which would help me tremendously with development of the project our company is currently working on.

Anyway, when do you think the demo software will be available?

-Gene

Posted on January 08, 2014 at 19:36

I know people who have it, so you might want to use classic support channels, like your local ST reps and FAEs

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..