cancel
Showing results for 
Search instead for 
Did you mean: 

How to play wav on STM32F4 Discovery?

antonius
Senior
Posted on January 09, 2014 at 01:20

Guys,

How to play wav on STM32F4 Discovery?

If I want to play from USB Key,

I enable :

#define MEDIA_USB_KEY

and how to connect USB flash drive to this board ? with adaptor ? the socket is too small for USB flash drive...

I'm reading ''Getting started...'' now it seems to be a cable ....

Is it reading from my PC or from USB flash drive....? I'm wondering ??

Thanks

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on January 09, 2014 at 01:53

and how to connect USB flash drive to this board ? with adaptor ? the socket is too small for USB flash drive...

http://www.ebay.com/bhp/micro-b-usb-host-otg-cable

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
antonius
Senior
Posted on January 09, 2014 at 04:40

and how can I define :

#define WAVE_NAME ''0:audio.wav''

for USB flash drive ?

thanks

antonius
Senior
Posted on January 09, 2014 at 04:58

I can't play every wav files, what's the limitation ?thanks

antonius
Senior
Posted on January 09, 2014 at 05:08

is it the limit ?

/* Audio file size and start address are defined here since the audio file is

    stored in Flash memory as a constant table of 16-bit data */

#define AUDIO_FILE_SZE          990000

so  I can't play 20Mbytes wav file ?

Posted on January 09, 2014 at 05:40

You have access to the same code and documentation I do. There may well be limits and types of files it can handle (bits, channels, frequencies, etc), or sizes/limits related to the convenience of coding. Some of these might be artificial or arbitrary. I haven't done the analysis.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..