Skip to main content
mailmail9116
Associate III
November 29, 2012
Question

STM3221G-EVAL : working with rs-232

  • November 29, 2012
  • 3 replies
  • 569 views
Posted on November 29, 2012 at 11:54

Hi All ,

I am working with STM3221G-EVAL board, i loaded the STM32F2-F4_Demonstration fw ,that came with the board ,i am trying to work with RS-232 , for now using this fw.

when i am trying to type on the LCD and send something back to my pc,it does nothing at all,the settings of the hyperterminal and the settings of the board are identical.

the jumper (jp22) is set to rs232 as instructed in the manual.

what am i missing? what else should i configure ?any other jumper or something?

if there is any other example that relevant only for configuring rs232 and sending data ,it will be mostly appreciated .

Thanks

Michael

#rs-232
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 29, 2012
    Posted on November 29, 2012 at 16:28

    // STM32 USART3 (Tx PC.10, Rx PC.11) STM3221G-EVAL - sourcer32@gmail.com
    #include ''stm32f2xx.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    /* --------------------------- System Clocks Configuration -----------------*/
    /* USART3 clock enable */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
    /* GPIOC clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /*-------------------------- GPIO Configuration ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    /* Connect USART pins to AF */
    GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3);
    GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3);
    }
    /**************************************************************************************/
    void USART3_Configuration(void)
    {
    USART_InitTypeDef USART_InitStructure;
    /* USARTx configuration ------------------------------------------------------*/
    /* USARTx configured as follow:
    - BaudRate = 115200 baud
    - Word Length = 8 Bits
    - One Stop Bit
    - No parity
    - Hardware flow control disabled (RTS and CTS signals)
    - Receive and transmit enabled
    */
    USART_InitStructure.USART_BaudRate = 115200;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    USART_Init(USART3, &USART_InitStructure);
    USART_Cmd(USART3, ENABLE);
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    USART3_Configuration();
    while(1)
    {
    while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART3, 0x49); // Send 'I'
    }
    while(1); // Don't want to exit
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mailmail9116
    Associate III
    December 2, 2012
    Posted on December 02, 2012 at 11:51

    Hi ,

    Thanks

    But i cannot compile the file,can you please maybe attach the whole project?

    thanks

    Tesla DeLorean
    Guru
    December 2, 2012
    Posted on December 02, 2012 at 17:00

    But i cannot compile the file,can you please maybe attach the whole project?

    I don't have this board, or know what tool chain you have. Can you not clone an existing project, strip it down and merge the basic example.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..