cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210C-EVAL: Application Example

stream77
Associate II
Posted on March 03, 2010 at 17:26

STM3210C-EVAL: Application Example

#utasker-stm3210c-eval #stm3210c-leds #lis302-accelerometer-lcd-demo
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Posted on January 16, 2012 at 15:05

The thread is nearly two years old, the newer date on subsequent posts reflects when the forum was rebuilt. The original posters are likely gone. Try contacting the one with the yahoo address directly.

If you are looking to run GCC under Windows, perhaps you should look at some of the WinARM packages, at least one has some STM32 example code, linker script and make file. There is also Yagarto and Code Sourcery, the latter has an STM32 targeted build as I recall.

Keil and IAR evals, code limited as they are, would still make for a relatively painless introduction to the STM32 family, with bundled examples and ST firmware library code.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hpipon957
Associate III
Posted on January 17, 2012 at 00:41

Hi

Also Rowely Crossworks is GCC based, as is ATOLLIC TrueStudio (Lite).

The uTasker project support the STM3210C-EVAL with these compilers, as well as IAR, Keil:

http://www.utasker.com/forum/index.php?topic=1697.0

It can be seen in operation here:

http://www.youtube.com/watch?v=2Rbz1SOoJVI

Regards

Mark