2009-05-03 9:06 PM
STM3210B with BLDC Motor?
2011-05-17 4:11 AM
Hi,
I recently bought the Development Kit STM3210B-MCKIT. I use it with the permanent-magnet synchronous motor FOC software library 2.0. Is this Kit also designed for the control of Brushless DC Motors with Hall Sensors? I think it is not yet optimized but it already works pretty well with a BLDC motor from Papst.