cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210B Not getting detected

shauns87
Associate II
Posted on September 10, 2014 at 22:09

Hi,

I have STM3210B and I am trying to connect it to PC. However, I am unable to connect it. I have installed all the STLink V2 drivers. Besides, I also download STVP tools as well, which installed its drivers.

When I insert the usb in my PC, I do not get the new hardware found window. When I check in Device manager, I am unable to find the device connected. 

Please help me identify the problem, so I can fix it.

Shashank
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
shauns87
Associate II
Posted on September 14, 2014 at 13:26

Hello Clive, 

I tried connecting it to all the ports to my laptop. I even used an another laptop to try but nothing happened,. 

I could be a problem with the cable but I am not sure, because I get the status light on, blinking in red, on the stlink V2 device. It means that the power is applied to the device with the cable. 

I will try to use the cable with my digital camera and see if the cable is able to communicate the my laptop. I will let you know if it works.

shauns87
Associate II
Posted on September 19, 2014 at 15:47

Hello Clive,

I got a new USB A to mini Cable of AWG 28 which is also used in blackberry mobile phones. I am able to successfully connect STLINK along with my STM3210B board.

Thanks for all your help.

Regards,

Shashank Sayanwar.