Question
STM32 TImer 2 Channel 3 ICU Config
Posted on May 12, 2015 at 21:42
I'm trying to configure the STM32F4 MCU to use Timer 2 Channel 3 as an Input Capture Unit to measure frequency on an external signal. But so far, I'm not able to trigger the interrupt:
static void TIM_Config(void) { TIM_ICInitTypeDef TIM_ICInitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; NVIC_InitTypeDef NVIC_InitStructure; //Enable and Set Timer 2 Interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //GPIO Config RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); palSetPadMode(GPIOB, 10, PAL_MODE_ALTERNATE(1)); //Timer 2 Config TIM_DeInit(TIM2); TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Prescaler = (STM32_SYSCLK / 1000000) - 1; // 1 MHz, from 48 MHz TIM_TimeBaseStructure.TIM_Period = 0xFFFFFFFF; // Maximal, TIM2 is 32-bit counter TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; // Rising/Falling/BothEdge TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInit(TIM2, &TIM_ICInitStructure); TIM_Cmd(TIM2, ENABLE); TIM_ITConfig(TIM2, TIM_IT_CC3, ENABLE); } void TIM2_IRQHandler(void) { if (TIM_GetITStatus(TIM2, TIM_IT_CC1) != RESET) { /* Clear TIM2_CH1 Capture compare interrupt pending bit */ TIM_ClearITPendingBit(TIM2, TIM_IT_CC1); } } #icu #stm32 #mcu #timer