STM32 Shutting down debug session
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-21 2:22 AM
I'm facing with a problem regarding debug session.
When I start debug session, after the configuration of USART2 the debug session is closed.
Keil message:
Cannot access target. Shutting down debug session
The shutdown occur with this instruction:
__HAL_AFIO_REMAP_USART2_ENABLE();
This is my configuration:
- STM32F103
- IDE Keil
- Keil project created with STM32Cube MX
- Debug Serial Wire with SWCLK, SWDIO, NRST.
- UART2 only TX and RX
Without debug the board works well, but I need the debug to solve some bug.
Thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-21 5:43 AM
And what does the code in that function actually do? Step into it.
Confirm AFIO and GPIOD clocks are enabled.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-21 6:02 AM
Hi clive1,
The code execute this macro/**
* @brief Enable the remapping of USART2 alternate function CTS, RTS, CK, TX and RX. * @note ENABLE: Remap (CTS/PD3, RTS/PD4, TX/PD5, RX/PD6, CK/PD7) * @retval None */ #define __HAL_AFIO_REMAP_USART2_ENABLE() SET_BIT(AFIO->MAPR, AFIO_MAPR_USART2_REMAP) GPIOD clock is enabled by this macro:__HAL_RCC_GPIOD_CLK_ENABLE();
This is the UART2 Init function:/* USART2 init function */
static void MX_USART2_UART_Init(void) { huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } } Inside the Init function there is this function's call to: /* Init the low level hardware */ HAL_UART_MspInit(huart); This function initialize the low level of UART2:else if(huart->Instance==USART2)
{ /* USER CODE BEGIN USART2_MspInit 0 */ /* USER CODE END USART2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PD5 ------> USART2_TX PD6 ------> USART2_RX */ GPIO_InitStruct.Pin = Debug_Serial_TX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(Debug_Serial_TX_GPIO_Port, &GPIO_InitStruct); GPIO_InitStruct.Pin = Debug_Serial_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(Debug_Serial_RX_GPIO_Port, &GPIO_InitStruct); //__HAL_AFIO_REMAP_USART2_ENABLE(); /* Peripheral interrupt init */ HAL_NVIC_SetPriority(USART2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); /* USER CODE BEGIN USART2_MspInit 1 */ /* USER CODE END USART2_MspInit 1 */ } And here the debug session fails.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-21 7:50 AM
Are you sure you don't have an issue externally with PD5? Could you scope the NRST pin and see what that does.
You could perhaps set the pin up as a GPIO and drive it high and low to see if that precipitates the same failure.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-22 12:25 AM
Hi clive1
I have the same problem. It seems that when I try to set a bit in AFIO->MAPR (for example AFIO->MAPR |= 0x30; the debug session fails. Do you have any idea why it fails? Thanks- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-22 12:57 AM
Hi clive1,
The GPIO PD5 in directly connected to an FTDI converter. Same thing for GPIO PD6.There aren't any components along these wires.This morning I will scope the NRST line to see what happen.Could this issue related to the remapping of UASART2 on PD5 and PD6?Thanks for your time.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-22 1:19 AM
Hi,
I found a temporary solution for you. You should useAFIO->MAPR |= AFIO_MAPR_USART2_REMAP | AFIO_MAPR_SWJ_CFG_JTAGDISABLE;
(in case of using SW) instead of using
__HAL_AFIO_REMAP_USART2_ENABLE();
I wonder if anyone can explain why the AFIO->MAPR value after the execution of following code is 0x04000030?!?
AFIO->MAPR = 0x02000000UL | 0x30; // The AFIO->MAPR value is 0x04000030 after execution of this line!!!
Bests,
Misagh
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-24 4:33 AM
Thanks Misagh92!
Your solution works! Now I can debug and read output form UART2.The only problem is connected to code generation performed by ST CubeMX. When I generate the project's code the__HAL_AFIO_REMAP_USART2_ENABLE()
is restored.
But this is not a big problem. Just keep it in mind.