2013-12-14 12:32 AM
I wrote 1 sn delay code for stm32 and ı used 168 mhz system clock.My delay cycle ıs 16000 for each ms and ıt work led blınk 1 sn.It dıdn't work when ıt was 168000 shouldn't it have worked at 168000 cycle.my code ıs
**** File : main.c**** Abstract : main function.**** Functions : main**** Environment : Atollic TrueSTUDIO(R)** STMicroelectronics STM32F4xx Standard Peripherals Library**** Distribution: The file is distributed “as is,�? without any warranty** of any kind.**** (c)Copyright Atollic AB.** You may use this file as-is or modify it according to the needs of your** project. This file may only be built (assembled or compiled and linked)** using the Atollic TrueSTUDIO(R) product. The use of this file together** with other tools than Atollic TrueSTUDIO(R) is not permitted.********************************************************************************//* Includes */#include ''stm32f4xx.h''/* Private macro *//* Private variables *//* Private function prototypes *//* Private functions *//****===========================================================================**** Abstract: main program****===========================================================================*/void delay_ms(int delay1){ delay1 = delay1*16000; while (--delay1) { }}int main(void){ GPIO_InitTypeDef GPIO_InitStruct; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_15 | GPIO_Pin_14 | GPIO_Pin_13 | GPIO_Pin_12; // we want to configure all LED GPIO pins GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; // we want the pins to be an output GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz; // this sets the GPIO modules clock speed GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; // this sets the pin type to push / pull (as opposed to open drain) GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; // this sets the pullup / pulldown resistors to be inactive GPIO_Init(GPIOD, &GPIO_InitStruct); // this passes the configuration to the Init function which takes care of the low level stuff /* Infinite loop */ while (1) { // if(1 == GPIO_ReadInputDataBit( GPIOA,GPIO_Pin_0)) // { // while(1 == GPIO_ReadInputDataBit( GPIOA,GPIO_Pin_0)); GPIO_SetBits ( GPIOD, GPIO_Pin_14) ; delay_ms(1000); GPIO_ResetBits (GPIOD, GPIO_Pin_14) ; delay_ms(1000); // } }}/* * Callback used by stm32f4_discovery_audio_codec.c. * Refer to stm32f4_discovery_audio_codec.h for more info. */void EVAL_AUDIO_TransferComplete_CallBack(uint32_t pBuffer, uint32_t Size){ /* TODO, implement your code here */ return;}/* * Callback used by stm324xg_eval_audio_codec.c. * Refer to stm324xg_eval_audio_codec.h for more info. */uint16_t EVAL_AUDIO_GetSampleCallBack(void){ /* TODO, implement your code here */ return -1;}2013-12-14 4:16 AM
If you are concerned about the processor speed, use the MCOx pins and output internal clocks, and measure them on a scope.
Observe that the processor in fact starts for a 16 MHz HSI clock, and has to be switched to something else, typically via SystemInit() in system_stm32f4xx.cFinally look at the assembler code generated by the compiler, and the optimization level selected. Unless you're writing code in assembler you probably have little control of cycle level performance.2013-12-15 12:11 AM
void delay_s
(int delay2)
{ delay2 = delay2*1680
00;
while (delay2--) { }} Delay(1000);it waits more than 10 second ı dıdn't understant why it waits more.ısn't ıt te same thing its like my main fuction has a diffrent clock speed from systemclock and it is like 8mhz or smtn like that2013-12-15 6:00 AM
The processor doesn't natively run C code, so assuming it's going to take a single cycle per loop iteration probably isn't going to hold water. To understand where the 10 cycles go you'll want to review the code output by the compiler.
2013-12-15 4:16 PM
''The processor doesn't natively run C code, so assuming it's going to take a single cycle per loop iteration probably (sic?) isn't going to hold water''
I'd say it is certainly not going to hold water!In fact, any assumption - unless fully qualified by compiler, version, and complete settings - about a direct correspondence from 'C' source lines to machine code is unlikely to hold water.http://www.8052.com/forum/read/162556
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.