STM32 I2C ''ACK Polling''
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-01-18 3:40 AM
Posted on January 18, 2012 at 12:40
Hi all,
I need an expert advice. How to poll for ACK from addressed Slave device? The background is, if the setup has a variable count of slaves and how to get the available slaves? The second case is the M24C64 EEprom. During the internal Write cycle, the device discon- nects itself from the bus, so I need to poll on ACK. But with my solution I get always an endless loop Between write byte and read byte function. If I use instead the do-while Delay(1) everything seems to be ok. This was very easy on an Atmega to check for ACk on device addessing, I've spent a lot of time to get this on STM32, but without success.void
eeprom_wait_for_ready (void) { /* unsigned char state = 0; do { while(I2C_GetFlagStatus(I2C_SELECTED, I2C_FLAG_BUSY)); // Send START condition I2C_GenerateSTART(I2C_SELECTED, ENABLE); // Test on EV5 and clear it while(!I2C_CheckEvent(I2C_SELECTED, I2C_EVENT_MASTER_MODE_SELECT)); // Sent slave address for write I2C_Send7bitAddress(I2C_SELECTED, EEPROM_I2C_ADDR, I2C_Direction_Transmitter); state = I2C_CheckEvent(I2C_SELECTED, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED); printf(''\r\n.''); I2C_GenerateSTOP(I2C_SELECTED, ENABLE); } while (!state); */ /**/ Delay(1); } Thx for helping.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0