2020-05-15 1:02 AM
Hello there,
So far I was designing only SPI masters in the STM32 MCU's- now I am doing a slave application and I am having problems.
First of, I was surprised that the STM32CubeF0-master repository doesn't consist of a single SPI slave example (please correct me if I am wrong).
I am trying to accomplish a simple functionality, that can be described as this:
For some reason, my config only works without using HAL_SPI_DMAStop. I am not sure how is using it breaking the program flow. Here is my function for slave SPI DMA management:
rc_t spis_manage(spis_t* const spis, const bool on)
{
UTIL_ASSERT(spis, e_rcPar);
rc_t stat;
if (HAL_SPI_STATE_READY != HAL_SPI_GetState(spis->hSpi))
{
if (e_rcOk != (stat = util_status(HAL_SPI_DMAStop(spis->hSpi))))
return stat;
}
if (on)
{
stat = util_status(HAL_SPI_TransmitReceive_DMA(spis->hSpi,
(uint8_t*)spis->bufTx, (uint8_t*)spis->bufRx, spis->size));
}
return stat;
}It is used as follows;
The incorrect behavior I am observing is that only the 1rst transfer is correct, i.e.
After I repeat the operation, it takes 3 bytes more pushed from the SPI master to trigger the transfer/ receive complete callback, and I dont know why.
Is my program flow correct? I would appreciate all help.
2020-05-16 1:46 PM
Yes, this seems right... I find this very problematic. Lets say the master asserts the NSS line and the slave gets ready to receive/ transmit X data. Master the transfers less bytes than X and deasserts NSS. Slave is stuck with old data in TX FIFO buffer and cannot do anything about it.
This is why I always send a dummy byte first, to flush that residue... This is a very dirty workaround.
2022-10-19 11:38 AM
hi! on the M0 + core, it worked for me only like this:
HAL_SPI_DMAStop(&hspi1);
__HAL_RCC_SPI1_FORCE_RESET();
__HAL_RCC_SPI1_RELEASE_RESET();
MX_SPI1_Init();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.