2009-11-24 7:13 PM
STM32 C/C++ build environment using CodeSourcery Sourcery G++
#fyi2011-05-17 3:25 AM
Great work lanchon, I wonder if you have any update since then.
I have tried compiling using the whole pack of ST-Arm_Toolchain_2.1 and it works fine except a few glitches(some minor, some major) and code size difference. This will be a great thing for my next Xduino (www.xduino.com) project to include a full IDE along with it so developer can use opensource IDE, compiler as well as opensource platform for simple programming. Did you find any bug in the compiler? I find some output differences from Keil and IAR (some how my serial port mysteriously starts with 7-bit mode instead of 8-bit and maybe other things I cannot fully confirm). Great work... :D and thank you.2011-05-17 3:25 AM
Hey!
First of all: lanchon great work! your linker scripts helped me a lot to get things working. But i have one little problem. I can debug in RAM or Flash and my application is working like it should(tested it with IAR workbench) but i can't get any interrupt. Why..? I used your stm32exceptions.c and .h file and put my code in it, but it still doesn't trigger any interrupt. Maybe your or someone has an advice for me... with kind regards -- rocky2011-05-17 3:25 AM
Hello all,
I downloaded arm-none-eabi-gcc (Sourcery G++ Lite 2009q1-161) 4.3.3 and tried the sample application from Lanchon's RC2 zip file in this thread - only LED is moved to RB1. But it does not work. I even tried simple LED blink application (listing is below). I am downloading the app by stm32 flash loader - so the chip works. I can read the data back. Does anybody have a clue what am I doing wrong ? 1.elf: file format elf32-littlearm Disassembly of section .text: 00000000 : 0: 00 08 00 20 21 00 00 00 b5 00 00 00 bd 00 00 00 ... !........... ... 00000020 : /* } */ volatile unsigned int icnt; int main ( void ) { 20: b480 push {r7} 22: b083 sub sp, #12 24: af00 add r7, sp, #0 unsigned char lpos = 0; 26: f04f 0300 mov.w r3, #0 ; 0x0 2a: 71fb strb r3, [r7, #7] GPIOB_CRL = 0x44444111; 2c: f640 4200 movw r2, #3072 ; 0xc00 30: f2c4 0201 movt r2, #16385 ; 0x4001 34: f244 1311 movw r3, #16657 ; 0x4111 38: f2c4 4344 movt r3, #17476 ; 0x4444 3c: 6013 str r3, [r2, #0] GPIOB_ODR = 0x00000005; 3e: f640 430c movw r3, #3084 ; 0xc0c 42: f2c4 0301 movt r3, #16385 ; 0x4001 46: f04f 0205 mov.w r2, #5 ; 0x5 4a: 601a str r2, [r3, #0] while( 1) { for(icnt = 0; icnt < 65000; icnt++) ; 4c: f240 0300 movw r3, #0 ; 0x0 50: f2c2 0300 movt r3, #8192 ; 0x2000 54: f04f 0200 mov.w r2, #0 ; 0x0 58: 601a str r2, [r3, #0] 5a: e00b b.n 74 5c: f240 0300 movw r3, #0 ; 0x0 60: f2c2 0300 movt r3, #8192 ; 0x2000 64: 681b ldr r3, [r3, #0] 66: f103 0201 add.w r2, r3, #1 ; 0x1 6a: f240 0300 movw r3, #0 ; 0x0 6e: f2c2 0300 movt r3, #8192 ; 0x2000 72: 601a str r2, [r3, #0] 74: f240 0300 movw r3, #0 ; 0x0 78: f2c2 0300 movt r3, #8192 ; 0x2000 7c: 681a ldr r2, [r3, #0] 7e: f64f 53e7 movw r3, #64999 ; 0xfde7 82: 429a cmp r2, r3 84: d9ea bls.n 5c lpos++; 86: 79fb ldrb r3, [r7, #7] 88: f103 0301 add.w r3, r3, #1 ; 0x1 8c: 71fb strb r3, [r7, #7] lpos &= 0x07; 8e: 79fb ldrb r3, [r7, #7] 90: f003 0307 and.w r3, r3, #7 ; 0x7 94: 71fb strb r3, [r7, #7] GPIOB_BRR = 0x0007; 96: f640 4314 movw r3, #3092 ; 0xc14 9a: f2c4 0301 movt r3, #16385 ; 0x4001 9e: f04f 0207 mov.w r2, #7 ; 0x7 a2: 601a str r2, [r3, #0] GPIOB_BSRR = lpos; a4: f640 4310 movw r3, #3088 ; 0xc10 a8: f2c4 0301 movt r3, #16385 ; 0x4001 ac: 79fa ldrb r2, [r7, #7] ae: 601a str r2, [r3, #0] b0: e7cc b.n 4c b2: bf00 nop 000000b4 : /* return 0; */ /* } */ void isr_nmi( void) { b4: b480 push {r7} b6: af00 add r7, sp, #0 b8: e7fe b.n b8 ba: bf00 nop 000000bc : while(1); } void isr_hardfault( void) { bc: b480 push {r7} be: af00 add r7, sp, #0 c0: e7fe b.n c0 c2: bf00 nop [ This message was edited by: vaclav.peroutka on 25-11-2009 08:46 ]2011-05-17 3:25 AM
Interrupt is a tricky one. Try the xduino library it has sources on simple implementation of interrupt along with examples on the site. : -) good luck...
2011-08-28 12:27 PM
The attachments are lost
Would it be possible to reattach them TIA Bingo2015-04-01 9:59 AM
Hi andreas1,
I saw in your postingm, that you have wrote a GDB STUB for the STM32. I am very interested in details, may the source code. I am looking for a long time for solution to have GDB connected to the target microcontroller without using JTAG or SWD. Would be happy to get an answer. Tom2015-04-01 11:45 AM
Understand that these posts are in fact from 2008, after at least two forum meltdowns, and rebuilds. And it's highly unlikely that these participants are monitoring the forum currently.