Skip to main content
gaurav2
Associate II
June 3, 2016
Question

STM Virtual Com Port Driver for Windows 10

  • June 3, 2016
  • 4 replies
  • 18963 views
Posted on June 04, 2016 at 01:21

I downloaded the VCP_V1.4.0_Setup.exe and ran it. But it only has Win7 and Win8 directories. 

Does anyone if either of them will work on 64-bit Windows 10? If neither will work then where can I get the STM VCP driver for Win 10?

Thanks!
    This topic has been closed for replies.

    4 replies

    mark239955_stm1
    Visitor II
    June 4, 2016
    Posted on June 04, 2016 at 08:54

    I got one of them working (sorry, can't remember which) on Win10 a few days ago.  It didn't auto-detect, I had to muck around and ''have disk'' etc but it did work.

    slimen
    Visitor II
    June 23, 2016
    Posted on June 23, 2016 at 11:19

    Hi,

    Please confirm if this problem still persists?

    May be compatibility mode can resolve this issue !

    Regards

    markpdbailey
    Visitor II
    August 22, 2016
    Posted on August 22, 2016 at 12:53

    The driver files will be installed at 

    C:\Program Files (x86)\STMicroelectronics\Software\Virtual comport driver\Win8

    Open a command prompt and cd into into this directory

    run

    dpintst_amd64 /LM

    Click yes on the driver installation boxes