cancel
Showing results for 
Search instead for 
Did you mean: 

stm uart communication voltage

IDANI.1
Associate

I want to use stm32f407gt with nextion touch screen. Display and stm will connect via to uart(Rx Tx pins). Stm work with 3.3V and nextion works with 5V. It will effect to communication ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KnarfB
Super User

STM app note AN4899:

"If the 5V UART interface input is TTL compatible, VOL<0.8V and VOH>2.0V. This implies that a 3.3V CMOS output can drive without any problem. An STM32 FT pad can accept 0V to 5V CMOS level input when VDD=3.3V."

FT = 5V tolerant pad.