STLink can not connect to Nucleo as ''Wrong device detected''
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-20 3:27 AM
Hello,
I am a new for STM32.
I bought Nucreo-L053R8 board, and installed latest Systemworkbench and STLink USB driver stsw-link009 on my PC. My OS is windows 8.1. I made a very short program and it could be compiled.
When I connect Nucreo board to my PC, I can see it as 'USB BUS DEVICE-STM32 STLink'.
Then I did run on Systemworkbench, then a window is opend and said 'OpenOCD Problem Occured, Reason: Wrong device detedted'.
After few second, USB is disconnected and I can see it as unknown device.
When I made the project, I select the device as L053.
Console shows like following.
-----------------------------------------
Wrong device detected
Open On-Chip Debugger 0.10.0-dev-00278-ga53935e-dirty (2017-05-09-09:25) Licensed under GNU GPL v2 For bug reports, readhttps://community.st.com/external-link.jspa?url=http%3A%2F%2Fopenocd.org%2Fdoc%2Fdoxygen%2Fbugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD adapter speed: 4000 kHz adapter_nsrst_delay: 100 Info : clock speed 4000 kHz Info : STLINK v2 JTAG v25 API v2 SWIM v14 VID 0x0483 PID 0x3748 Info : vid/pid are not identical: 0x0483/0x374B 0x0483/0x3748 Info : using stlink api v2 Error: init mode failed (unable to connect to the target) in procedure 'program' in procedure 'init' called at file 'embedded:startup.tcl', line 473 in procedure 'ocd_bouncer' ** OpenOCD init failed ** shutdown command invoked-----------------------------------------
Let me know how should I do.
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-21 8:01 AM
Right, almost every nucleo I bought had an old firmware version causing ST_LINK issues. I have not mentioned it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-20 8:19 AM
Maybe wrong configuration - you have ST-LINK v2 but you actually has v-1 in cfg file.
stlink-v2.cfg:
VID/PID 0x0483 0x3748 for ST-Link/V2
VID/PID 0x0483 0x374b for ST-Link/V2-1- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-20 9:31 PM
Bogdan,
Thank you for your reply.
I changed the config file as ST-Link/v2, and the error massage of
'
Info : vid/pid are not identical: 0x0483/0x374B 0x0483/0x3748'
is disappered. but the result is still same.
My board usb hardware infomation's PID is 0x3748, so my board is ST-Link/v2 for sure.
And I noticed that, the log said,
'
Info : STLINK v2 JTAG v25 API v2 SWIM v14 VID 0x0483 PID 0x3748'
so it will connect as SWIM, but my project debug config has
'transport select 'hla_swd'
that mean I think the config setting is SWD but the hardware is SWIM.
If this is the problem, how can I change the config from SWD to SWIM? I tried to change the hla_swd to hla_swim, but when I build it, the swim character is change to swd automatically.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-21 1:18 AM
Dear Takayoshi Ishii,
You said 'that mean I think the config setting is SWD but the hardware is SWIM.',but ALL STLink/V2-1 in Nucleo uses SWD interface despite supporting JTAG/SWD/SWIM.Currently OpenOCD cfg's default SWD clock settings for L0 is too fast,
so you need to reduce clock below 1000kHz.I met same problem STM32L053C8-Discovery,and avoid the error to reduce SWD clock.
See my article for more information.
http://nemuisan.blog.bai.ne.jp/?eid=222175
Best Regards,
Nemui.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-21 6:45 AM
Nemui san,
Thank you for the infomation!
Finally, I could program it as following.
1) Update the ST-Link firmware. The Nucleo that I bought was old ST-Link firmware.
2) Set the Clock lower than 1000KHz. On the Systemworkbench, Run->RunConfigurations->Debugger->Show generator options->Frequency tab->480KHz
Thank you very much for all your guys!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-21 8:01 AM
Right, almost every nucleo I bought had an old firmware version causing ST_LINK issues. I have not mentioned it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-05 5:06 PM
Hey, I'm having a similar error (granted its a different chip, and not a development board, I'm using a custom board...) How do I change the stlink config file? I can't even find it in my project. I see it linked in the project.cfg file at the top like this:
source [find interface/stlink.cfg]
But I can't fin stlink.cfg... I've also attached the errors I'm having. They look similar to yours.
Open On-Chip Debugger 0.0-dev-00005-g4030e1c-dirty (2017-10-24-07:56)
Licensed under GNU GPL v2
For bug reports, read
/external-link.jspa?url=http%3A%2F%2Fopenocd.org%2Fdoc%2Fdoxygen%2Fbugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 950 kHz
adapter_nsrst_delay: 100
Info : clock speed 950 kHz
Info : STLINK v2 JTAG v29 API v2 SWIM v7 VID 0x0483 PID 0x3748
Info : vid/pid are not identical: 0x0483/0x374B 0x0483/0x3748
Info : using stlink api v2
Info : Target voltage: 3.258614
Info : Stlink adapter speed set to 950 kHz
Info : STM32F030R8Tx.cpu: hardware has 4 breakpoints, 2 watchpoints
Info : Stlink adapter speed set to 950 kHz
adapter speed: 950 kHz
Error: timed out while waiting for target halted
TARGET: STM32F030R8Tx.cpu - Not halted
in procedure 'program'
in procedure 'reset' called at file 'embedded:startup.tcl', line 478
in procedure 'ocd_bouncer'
** Unable to reset target **
shutdown command invoked
Your help would be veryappreciated!
EDIT: I tried running it as Debug. This is what I got:
Open On-Chip Debugger 0.0-dev-00005-g4030e1c-dirty (2017-10-24-07:56)
Licensed under GNU GPL v2
For bug reports, read
https://community.st.com/external-link.jspa?url=http%3A%2F%2Fopenocd.org%2Fdoc%2Fdoxygen%2Fbugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 950 kHz
adapter_nsrst_delay: 100
Info : tcl server disabled
Info : telnet server disabled
Info : clock speed 950 kHz
Info : STLINK v2 JTAG v29 API v2 SWIM v7 VID 0x0483 PID 0x3748
Info : vid/pid are not identical: 0x0483/0x374B 0x0483/0x3748
Info : using stlink api v2
Info : Target voltage: 3.255445
Info : Stlink adapter speed set to 950 kHz
Info : STM32F030R8Tx.cpu: hardware has 4 breakpoints, 2 watchpoints
Info : accepting 'gdb' connection on tcp/3333
Info : Stlink adapter speed set to 950 kHz
adapter speed: 950 kHz
Error: timed out while waiting for target halted
TARGET: STM32F030R8Tx.cpu - Not halted
in procedure 'reset'
in procedure 'ocd_bouncer'
Info : device id = 0x20006440
Info : flash size = 64kbytes
Info : Stlink adapter speed set to 950 kHz
adapter speed: 950 kHz
Error: timed out while waiting for target halted
TARGET: STM32F030R8Tx.cpu - Not halted
in procedure 'reset'
in procedure 'ocd_bouncer'
Info : Stlink adapter speed set to 950 kHz
adapter speed: 950 kHz
Error: timed out while waiting for target halted
TARGET: STM32F030R8Tx.cpu - Not halted
in procedure 'reset'
in procedure 'ocd_bouncer'
Error: Target not halted
Error: failed erasing sectors 0 to 2
Error: flash_erase returned -304
shutdown command invoked
Error in final launch sequence
Failed to execute MI command:
load /Users/mahmudahmad/Desktop/Development/STM/testing/Debug/testing.elf
Error message from debugger back end:
Error erasing flash with vFlashErase packet
Error erasing flash with vFlashErase packet