cancel
Showing results for 
Search instead for 
Did you mean: 

Stemwin Library Integration

sruthi
Associate II
Posted on August 30, 2016 at 09:22

 I am trying to integrate STemWin_Library_V1.1.2 with my code in Keil uvision4(My controller is STM32F10VCT6 and display controller is SSD1963).But while compiling and linking shows  an error .\Obj\l1651_lcd.axf: Error: L6218E: Undefined symbol GUI_Init (referred from main.o). Is there any solution for this? 

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
slimen
Senior
Posted on August 30, 2016 at 10:59

Hi,

I think the Undefined symbol error means that your application does not include source, libraries or object which including the function. 

You should review the configuration of your project, and make sure that your project contains all the required library source files.

Regards

sruthi
Associate II
Posted on August 31, 2016 at 06:16

Thank you for your reply and there is no such source files which including the function.I have added all library files shared in 

STemWin_Library_V1.1.2 to my project.But still that error remains.What should I do? May I need to purchase any other library files from STMicroelectronics. I am sorry actually I don't have much knowledge in this(Beginner).Can you help me?

Walid FTITI_O
Senior II
Posted on August 31, 2016 at 11:34

Hi sruthi,

I recommend you that you open a ready example and compare the workspace there (files, included paths..) as ''STemwin_SampleDemo'' from STM32CubeF4 at this path: STM32Cube_FW_F4_V1.12.0\Projects\STM324xG_EVAL\Applications\STemWin\STemWin_SampleDemo

for GUI_init() Check the following path if it is included: ..\..\..\..\..\..\Middlewares\ST\STemWin\inc

When including your paths, give attention to the position of each file regarding the project folder.

-Hannibal-

sruthi
Associate II
Posted on September 07, 2016 at 14:08

sruthi
Associate II
Posted on September 07, 2016 at 14:12

Hi,

Actually I was working with keil 4(IDE) earlier, now upgraded to keil 5, the code is successfully compiling now.And flash also successfully done.But LCD is not responding.Should I make any changes in GUIDRV_FlexColor.h?? As I said my lcd controller is SSD1963 and the communication is through FSMC. I think the problem is with LCD controller initialization. Can you help me?

slimen
Senior
Posted on September 08, 2016 at 00:13

Hi,

Did you set up correctly initialize ssd1963 controller?

You should define GUIDRV_FLEXCOLOR_F66720 to use ssd1963 controller.

Look at this 

http://www.st.com/content/ccc/resource/technical/document/application_note/54/c9/95/42/8c/0b/43/69/DM00089670.pdf/files/DM00089670.pdf/jcr:content/translations/en.DM00089670.pdf

 it maybe helpful for you.

Regards