cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin application for STM32H735G-DK

ilariari
Associate II

Hello!

Dealing as newbie with STM32 MCUs, I'm focusing on projects of STM32Cube_FW_H7_V1.8.0 packet.

As my goal is to develop on STM32H735G-DK, I'd need an application or an example which uses STemWin library. Unfortunately I can't find such a combination in STMCube (STemWin for STM32H735G-DK).

Editing a project which links STemWin in order to use it for another DK/MCU seems to be foreclosed as MCU and Board settings are disabled in the C/C++ Build/Settings/MCUSettings section of Project Properties.

Thank you very much for giving me some hint!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0