cancel
Showing results for 
Search instead for 
Did you mean: 

Standby mode and alarm strange problem

sami
Associate II
Posted on July 25, 2013 at 10:11

Hello

After producing the first 100 products for the customer , we noticed that 10% of the products around 10 units getting faults.

Our products wakeup from wakeup pin  then after operation it goes to standby mode waiting again a wakeup button to be pressed , and also everyday at certian  fix time it wakes up from the alarm of RTC . we noticed about 10 %  of the units  when wakes from RTC alarm the stm32f407 get stucks some where .. and cannot be closed waiting a reset only ...

the strange thing when waking up from wakeup pin all is ok ... and no problem .

we have been duging for a week.. is it bug of STM32f4 with RTC alarm and standby .. or what i am doing wrong here ..

Thank you in advanced
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 25, 2013 at 22:49

Dear gentlemen,

Yes, we confirm the limitation. We recently ( 2 months ago ) added in our official errata

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/DM00037591.pdfhttp://

Details in Section 2.1.5, We have a solution or let's say a workaround to modify the sequence of entry code to Standby mode to avoid that lockup situation. the entry logic is level sensitive and not edge, So if the external source is high, the RTC alarm will not be seen and also other sources, except reset.

Cheers,

STOne-32