ST-Util GDB Server Quit Unexpectedly. See gdb-server output for more details.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-03 12:54 AM
Hi,
I'm want to do a step by step debug of the project "https://github.com/aws/amazon-freertos"/(varient), I have installed VM on windows 10 and using vs code I want to do a step by step debugging. I have installed the GDB and all relevant tools in ubuntu 18. The launch file for the same is -
{
// Use IntelliSense to learn about possible attributes.
// Hover to view descriptions of existing attributes.
// For more information, visit: https://go.microsoft.com/fwlink/?linkid=830387
"version": "0.2.0",
"configurations": [
{
//"cwd": "${workspaceFolder}/hotwater-fw/",
"cwd": "${workspaceFolder}",
"executable": "/home/suman/sandbox/hotwater-fw/build/aws_demos.elf",
//"executable": "/hotwater-fw/build/aws_demos.elf",
"name": "Debug hotwater code",
"request": "launch",
"type": "cortex-debug",
"runToEntryPoint": "main",
"showDevDebugOutput": true, //"none",
//"servertype": "openocd",
//"servertype": "stlink",
"servertype": "stutil",
"gdbpath": "/usr/bin/gdb-multiarch"
}
]
}
When start debugging in vscode using F5/Run->Start Debugging I get a error with below text in debug terminal-
Reading symbols from arm-none-eabi-objdump --syms -C -h -w /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
Reading symbols from arm-none-eabi-nm --defined-only -S -l -C -p /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
Launching GDB: arm-none-eabi-gdb -q --interpreter=mi2 /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
Set "showDevDebugOutput": true in your "launch.json" to see verbose GDB transactions here. Helpful to debug issues or report problems
Launching gdb-server: st-util -p 50000 --no-reset
Please check TERMINAL tab (gdb-server) for output from st-util
Finished reading symbols from objdump: Time: 304 ms
ST-Util GDB Server Quit Unexpectedly. See gdb-server output for more details.
I did change the server to ST-Link but the error remains as shared below -
Reading symbols from arm-none-eabi-objdump --syms -C -h -w /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
Reading symbols from arm-none-eabi-nm --defined-only -S -l -C -p /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
Launching GDB: arm-none-eabi-gdb -q --interpreter=mi2 /home/suman/sandbox/hotwater-fw/build/aws_demos.elf
1-gdb-set target-async on
Setting GDB-SErver CWD: /opt/st/stm32cubeide_1.9.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_2.0.200.202202231230/tools/bin
Launching gdb-server: /opt/st/stm32cubeide_1.9.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_2.0.200.202202231230/tools/bin/ST-LINK_gdbserver -p 50000 -cp /opt/st/stm32cubeide_1.9.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.0.200.202202231230/tools/bin --swd --halt
Please check TERMINAL tab (gdb-server) for output from /opt/st/stm32cubeide_1.9.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_2.0.200.202202231230/tools/bin/ST-LINK_gdbserver
Finished reading symbols from objdump: Time: 236 ms
ST-LINK GDB Server Quit Unexpectedly. See gdb-server output for more details.
Can you please help me resolve the same.