cancel
Showing results for 
Search instead for 
Did you mean: 

ST‑LINK V3 Minie connects to STM32F100RBT6B Discovery but not to my custom board

saran
Associate II

I’m using an ST‑LINK V3 Minie with an STM32F100RBT6B Discovery board (which also has an STM32F103C8T6), and it works perfectly. However, when I connect the same ST‑LINK V3 Minie to my custom board that uses the same STM32F100RBT6B chip, it fails to connect.

I’ve wired VCC (VTref), GND, NRST, TMS/SWDIO, and TCK/SWCLK exactly as specified.

Black - Ground

White - Vcc

Yellow - Reset

Blue - Clock

Purple - TMS

On the Discovery board this setup works fine, but on my custom board the debugger cannot establish communication.

Could anyone suggest what additional checks I should perform on the custom board?

 

 

1 REPLY 1
Ozone
Principal II

Doesn't this suggest the problem is with your custom board ?

I would suggest to connect the VDD /T_Vcc pin as well, as it is used to sense of the target is powered :

Ozone_0-1764569768155.png

Have you checked the voltage at the supply pins of you custom board (at the MCU pins), and the power consumption ?
Only then would I connect an external tool like a debug adapter.